Other Parts Discussed in Thread: TPA3004D2 , TPA2008D2 Dear Sir
We will use one audio amp solution to design stereo BTL (3W/8ohm) and PBTL (10W/6ohm) ,but PBTL and BTL will not use at the same time
But we need have volume control function just like TPA3004D2…
Hi Mehrdad,
I can see in your schematic that you have a TPA2008D2 integrated in your application.. It seems that you've configured PCM2704C in Bus-Powered 500mA, but there is a TPA2008D2 sharing this supply so maybe the USB power can't supply both devices…
Dear sir,
In some posts, i read an tpa2008d2 can be used for an pre amplifier for tas5622A, is it possible to interface or not?, please replay to me sir.
Thanks & Regards
Kiran
Other Parts Discussed in Thread: TPA2008D2 , PCM2912 , PCM2912A , TPA2025D1 I put together PCM2912A and TPA2008, USB to Class D Audio. I have duplicated the PCM2912A circuit as shown in SLES230-SEPT 2008 AND sba141 guide. When plugged into my USB port, not…
Hi Anthony,
That's really cool!, we have plenty options on the low power amplifier selection, you may take a look to our Audio Selection Tool . Do you prefer a mono or stereo amplifier?, you can take a look to our TPA2025D1, this device features an…
Hi Rahul,
Both Ri must be varied in the same values, so there is not a recommended way to control the gain of the TPA2005D1 with a single potentiometer; although you can use a dual potentiometer to control both Ri but keep special care on the precision…
Other Parts Discussed in Thread: PCM2912 I put together PCM2912A and TPA2008, USB to Class D Audio. I have duplicated the PCM2912A circuit as shown in SLES230-SEPT 2008 AND sba141 guide. When plugged into my USB port, not recognized because it is not downloading…
Hi, Chitu,
TPA2008D2 will work as a modulator, just connect the two outputs to the two inputs on the TAS5631. Just make sure you run the TPA2008D2 at 4.2V or less, or you'll damage the input pins on the TAS5631. I'd recommend 3.3V.
And, you're…