Part Number: TPA2011D1
Tool/software:
We want to use a square wave 1KHz for Audio AMP input that is mean digital signal for input, not analog signal, Is it ok?
Part Number: TPA2011D1 Tool/software: Hi team,
Customer would like to use TPA2011D1 in their application.
They need output DC protection, however, TPA2011 don't get this feature.
Do we get any mono 2W~6W, analog input audio amp part with output…
Part Number: TPA2011D1 Other Parts Discussed in Thread: TPA6211A1 Tool/software: Hi
Do you have any suggestions for materials that can replace aw8733 with the same function?
DS_AW8733A_EN_V1.1.pdf
This example is built-in BOOS
T You can also recommend…
Part Number: TPA2011D1
Hello
I am currently using a class D audio amp that can provide 3 W of output power, has a voltage range between 2.8 and 6 V, and has 3 ohms of load (I don't have the part number). I found the TPA2011D1 as a possible alternative…
Part Number: TPA2011D1 Other Parts Discussed in Thread: TPA2005D1 , TPA2013D1 Hi,
I'm looking for a speaker amplifier with the following specs. From what I've searched, the TPA2x series seems to be the one, but are there any products you recommend?…
Part Number: TPA2011D1 Hi team,
When using long cables (up to 100m) with filter-less amplifiers like the TPA2011D1, is it advisable to have a separate filter? Also, please tell me how to calculate the filter in such a case. Also, are there any class…
Part Number: TPA2011D1 Hello team,
My customer is trying to use TPA2011D1 with the configuration as Figure 31 on the datasheet.
However, the IN+ is connected instead of IN-. Is this configuration correct?
Shouldn't it be IN- connected to GND?…
Part Number: TPA2011D1 I've connected the TLV320AIC3104IRHBR's LEFT_LOP/M to the TPA2011D1YFFT and set the Gain to 2V/V.
The LEFT_LOP/M outputs 4Vp-p, but the TPA2011D1YFFT only outputs 6Vp-p.
Please assist me in reviewing the schematic to identify…
Part Number: TPA2011D1 Hello TI,
There are oscillations observed on output of power amp around 300kHz measured by oscilloscope and then with NF probe using spectrum analyser, to be sure there is no parasitic circuit added to the output of amp.
Any…
Part Number: TPA2011D1 I could not find in the datasheet the timing associated with the enable pin, i.e., how long it takes for the device to be enabled and disabled with the assertion of the enable pin. I am not asking about the startup time, well described…