Part Number: TPA2011D1 Other Parts Discussed in Thread: TAS2110 When EN is set high, device starts cycling, with a large current spike on VDD every 100 msec. It looks like it's drawing high inrush current, then short circuit shutdown and auto-recovery…
Part Number: TPA6130A2 Other Parts Discussed in Thread: TAS2110 , TPA2011D1 , TAS2572 Tool/software: Hi ti team,
Please recommend an earphone amplifier IC with the following requirements:
Headphone amplifier requirements: 32 ohm load @ 450mW, Class D or…
Hi Cevdet,
I would suggest using the headphone output rather than speaker output signal. Speaker output may be a PWM-like signal, while headphone should be analog signal which is better for analog input amplifiers such as LM48511 or TPA2011D1.
Best re…
Part Number: TPA2011D1 Dear Team,
Our customer was feedback that they can hear some pop/click noise when they stop the audio streaming.
We had measure the waveform and we found TPA2011D1 didn't shutdown the output immediately when enable pin pull-low.
The…
Part Number: LM48511 Other Parts Discussed in Thread: TPA2011D1 , TPA2013D1 Tool/software: 1. When was this device launched? Also, until when is supply guaranteed?
2. Are there any recommended replacement parts?
Part Number: TPA2011D1 Other Parts Discussed in Thread: TPA2028D1 , TAS2563 , TAS2557 , TPA2026D2 Hi team,
We want to find an audio amp,the requirement as follow:
Requirements drive 4 euro 3W/5W, 5V input, small harmonic distortion, anti-breaking sound,…
Part Number: TPA2011D1 Hello team,
My customer need a 5W mono class D amplifier, what's the best choice that you would recommend? Or do I need to look into a middle power device?
I'm asking here because I'm having some trouble accessing your roadmap…
Part Number: TPA2011D1
customer use 2x 8ohm; 1W speaker connected in parallel( impedance equivalent to 4ohm speaker) for TPA2011D1 and they would like TPA2011D1 support around 10x gain.
What is the input resistance; RI; we recommend for TPA2011D1? So…
Part Number: TPA2011D1 Hi Team,
Is there an equation to calculate the maximum output power for TPA2011D1?
My customer is asking what would be the maximum output power under the below condition:
Vdd: 2.7V, 4ohm speaker.
Best regards,
Andy Chu