Part Number: TPA2012D2 Hi all,
I have a quick question for TPA2012.
Input bias voltage of TPA2012 is 0V in shut down mode? (input bias circuit is not active in shut down mode?)
Best regards,
Part Number: TPA2012D2 Dear Support team,
Please tell me about the input impedance of TPA2012D2 under shutdown mode.
When the SDL-pin and/or SDR-pin are driven low, the system enters shutdown mode. Does the input impedance determined by the gain setting…
Part Number: TPA2012D2 Other Parts Discussed in Thread: TLV320AIC3106 Hello,
We have an audio configuration where we use TLV320AIC3106 as the Audio Codec, which is driving the TPA2012D2 Class D amplifier.
We are routing the MONO_LOP/M differential lines…
Part Number: TPA2012D2 Hello, we use TPA2012 to drive 1W speakers. I am attaching the circuit diagram below. IC is 5vdc supplied. It seems working but sometimes it gives continuous 5VDC to the speakers for no reason and speakers are heating so much so…
Part Number: TPA2012D2 Hi Team,
Customer is using TPA2012d2 and find that there is a pop-click issue. Do we have any recommendation to solve it or any other device can we recommend to customer?
Regards,
Nic
Part Number: TPA2012D2
Hi,
SNR of TPA2012D2 is 95dB in HP. Please let me know it test condition. (I didn't found it when I refered to datasheet.)
Best Regared, Y. Hirata
Part Number: TPA2012D2 Hello,
as shown in the title i use the TPA2012D2 to amplify the signal witch comes from a WL8731L Audio Codec (HPLOUT/HPROUT). (G0 - High / G1 - Low) --> Gain (4) 4V/4V / dB 12
I coupled the input with resistors and capacitors…
Part Number: TPA2012D2 Other Parts Discussed in Thread: TPA2016D2 , TPA2026D2 , , Hi Team,
On the TPA2012, we require is to be able to detect if a short circuit event has occurred. Since this IC does not have a FAULT pin, we were wondering if there is any …
Part Number: TPA2012D2 Other Parts Discussed in Thread: TPA2016D2 , TPA2026D2 Hi,
I am planning to use the TPA2012D2 in a relatively high volume consumer device but noticed that the eval module for the TPA2012D2 is labeled as obsolete on all major distributors…
Part Number: TPA2012D2 Hi all ,
customer found that when each time when power on , they always hera a sound of "pop" . Here is the related sch. Is the OUTPUT status are undifined when power on? Is there any way to eliminate it ?
Could you help…