Other Parts Discussed in Thread: TPA2013D1 The datasheet for the TPA2013D1 does say that it includes a built-in low pass filter. But I can't find any information in the datasheet that would tell me what the properties of that filter are.
I'm generating…
Other Parts Discussed in Thread: TPA2013D1 I have an audio amp circuit using the TPA2013D1 and entire device is failing FCC Part 15 conducted AC noise with a spike at 3.31MHz. If I disable the audio amp or disconnect the speaker, the spike disappears…
Other Parts Discussed in Thread: TPA2013D1 Dear sir,
My question is : What the power the audio PA refers to ?? the output power?
I want to how to calculate out the power,, Which factors will determinate the power, the power source, the load and the…
Hello. I'm using the TPA2013D1RGPR with recommended ferrites and 1000pF caps but the noise at the speaker output is enormous! 50% duty cycle, square wave at 290kHz 4.5Vpp with the input audio grounded (on the far side of the caps). With audio running…
I have used this chip for the first time and had great expectations about it. Unfortunately I receive a very significant noise from the output and I don't know why.
My circuit is not much different than the application example in the datasheet. I drive…
Other Parts Discussed in Thread: TPA2013D1TPA2013D1 provides constant output power even with falling battery voltage, by combining a class-D amplifier and a boost converter to produce a stable power supply at a higher voltage than the battery. It requires…
Part Number: LM48511 Other Parts Discussed in Thread: TPA2011D1 , TPA2013D1 Tool/software: 1. When was this device launched? Also, until when is supply guaranteed?
2. Are there any recommended replacement parts?
Part Number: TPA2011D1 Other Parts Discussed in Thread: TPA2005D1 , TPA2013D1 Hi,
I'm looking for a speaker amplifier with the following specs. From what I've searched, the TPA2x series seems to be the one, but are there any products you recommend?…
Part Number: TPS62160 Other Parts Discussed in Thread: TPA2013D1 hi Team:
TPS62160 Vin voltage is 6-8.4V,output voltage is 5V, and the load is TPA2013d1,at - 20 ℃ ,the TPS62160 output voltage is 2-3V? why?