Part Number: TPA2016D2 Other Parts Discussed in Thread: TPA2018D1
Hi,
We're using an array of TPA2016D2s to drive multiple coils (one coil per IC) on a very dense PCB, so minimizing routing is critical. Frequencies are from 20Hz to 15KHz.
Only the…
Part Number: TPA2016D2 Tool/software: how to set TPA2016D2 DRC
The specification states that with a 5V power supply, the power corresponding to 1% distortion is 2.5W. However, even when the limiter power level is maximized, the output can only reach…
Part Number: TPA2016D2 Tool/software: Hi team,
Can this device be used with a single-ended output? If so, is it sufficient to add a ferrite bead or LC filter to the output? Also, please advise on how to handle the OUT pin if it can be used.
Best Regards…
Part Number: TPA2016D2 Tool/software: Hello,
I'm using the TPA2016D2 in a voice amplifier application. The signal chain is pretty straightforward. Microphone -> class AB output from preamplifier -> TPA2016D2 -> two 8 ohm speakers, one on L channel,…
Part Number: TPA2016D2 Dear TI Teams,
We have some question about the PA use of TPA2016D2. We have noticed that there some relevant descriptions in the datesheet, but the explanations are seems not very specific. Can you help to check the following…
Part Number: TPA2016D2 Dear TI Engineer,
We have some question about the Gain Limiter Level in the TPA2016D2 debug tools. We want to know what is the principle of this limiter in PA? Is it dynamic gain control (dynamic reduction of gain for large…
Part Number: TPA2016D2 Tool/software: I have a pcb design with two TPA2016D2 devices on board. Having separate i2c busses is not an option here. I only have one i2c bus.
PDF clearly states that the i2c address can be changed, but it doesn't say how…
Part Number: TPA2016D2 There are two questions about audio amplifier TPA2016D2 as follows.
1. Output power [W] versus THD+N [%] curves are drawn on the datasheet of TPA2016D2. Could you let me know the measurement conditions as detailed as possible…
Part Number: TPA2016D2 Hi, team I'm using TPA2016D2 for one of my project I'm not able to configure negative dB settings .
1. I tried all methods given in datasheet setting Compression ratio and setting the all registers WRT data sheet But i'm not able…
Part Number: TPA2016D2 Tool/software: The datasheet for this audio amp includes the following text:
Some of the default values can be reprogrammed through the I2C interface and written to the EEPROM. This function is useful to speed up the turnon time…