Other Parts Discussed in Thread: TPA2016D2 Hi you,
I am using TPA2016D2 designing a audio amplifier for personal device. In the Datasheet, TPA2016D2 can produce 1,7W at 8Ohm load, but in my design it have just been 0,4W. What is the problem?
Thanks al…
Other Parts Discussed in Thread: LM4674 , TPA2016D2 I am looking for a power amp to drive our Hi-Z (40 Ohm, 16 mH) headphone driver. I got samples of the TPA2016D and built a prototype board; the board drives a 8 Ohm speaker well enough, but when connected…
Other Parts Discussed in Thread: TPA2016D2 Hi,
the tpa2016d2's datasheet mentions that there is an eeprom which stores the default setting. On page 22 it is said that for faster start-up time it is possible to change those default values.
Is there…
Other Parts Discussed in Thread: TPA2016D2 Hi,
I am using the AIC3204 codec with the TPA2016D2 Audio amplifier. Is there any difference between the AIC3204 and the TPA2016D2 DRC performaces ?
My taget audio application is focused on voice.
Thanks.
…
Other Parts Discussed in Thread: TPA2016D2 Hi,
Are there any other drivers for TPA2016D2 other than the EVM files?
We are using Linux 2.6.35.
Thank you,
CJH
Other Parts Discussed in Thread: TPA2016D2 Hello,
i want to control volume via TPA2016D2 for my application. i downloaded the Tool for EVM and saw on the volume control panel help that fixed gain, max gain and limit level should be set in tandem but i…
Other Parts Discussed in Thread: TPA2016D2 , TPA6130A2 Hi all, When TPA2016D2 and TPA6130A2 set to the hardware shut down mode, is the I2C bus condition Hi-Z? Regards, Toshi
Other Parts Discussed in Thread: TPA6130A2 , TPA2016D2 , TPA6120A2 Hi,
I am using AIC3204 differential HP+/HP- outputs (1 channel) to drive both Left and Right TP6130A2 and TPA2016D2 audio amplifier inputs pins.
I have to use Boths dual (Left and Right…
Other Parts Discussed in Thread: TPA2016D2 , TPA2012D2 Hello,
I would like to make this application stereo where the left channel power only the left speaker and the right channel the right speaker using the TPA2016D2.
Right now the design is Mono.
The…