Part Number: TPA2028D1 Hi
Can I use TPA2028 for both products?
One set of speakers is connected to 2W/4Ω (set Max.<2.5W)
The other group is connected to the speaker 1W/7Ω (set Max.<0.02W)
Part Number: TPA2028D1 Hello I am Luis
Let me ask a question.
I have a question TPA2028D1 volume control
[test circuit]
input 1kHz sinewave to IN+, IN- and attach RC filter(R-1kohm, -4.7nF) to OUT+, OUT -
and input signal 1kHz sinewave and output is also…
Part Number: TPA2028D1 Hello I am Luis
Let me ask a question.
I wanna to show TPA2028D1 1kHz sinewave
first input 1kHz sinewave to IN+, IN- and attach RC filter(R-1kohm, -4.7nF) to OUT+, OUT - but I cannot output 1kHz sinewave ? what's wrong??
how…
Part Number: TPA2028D1 Hi all,
As described, due to PCB layout and restrictions, I use 3.3V for I2C and a 5V on EN pin, tied to PVDD.
I ask because I get NAK when communicating to TPA2028D1.
Does it matter these levels differ and can that be the answer…
Part Number: TPA2028D1 HI Team
We are using the TPA2028D1YZF in one of our project. We are seeing some white noise coming form the speaker.
Below is the cases:
1. When we enable the amplifier there is some pop sound coming every time.
2. When we make…
Part Number: TPA2028D1 Hello team,
I received a question about circuit pattern of audio amp. I would appreciate it if you could take a look and give us some feedback. Any brief feedback would be fine.
Their main concern are about line width. Please refer…
Part Number: TPA2028D1 Hello TI Forum,
I am looking for a replacement for the TPA2028 since it is currently not available anywhere. Would the pin compatible TPA2018 be an option for this? What are the main differences between these two amplifiers?
Is…
Part Number: TPA2028D1
Hello all,
I am currently using the TPA2028D1 in my application / custom prototype PCB and are pretty satisfied with the control as well as the output. The amplifier is directly powered through an attached 3.7V 1S LiPo-Battery…