SS Jung,
As I mentioned the AGC is working all the time in this application, but that should be only working when the output signal exceeds the limiter level due to transients high spikes until the output signal comes back to its normal level (the normal…
Part Number: TPA2028D1YZFEVM I have procured a TPA2028D1YZFEVM and working on windows 10 OS. I have installed the TPA2028D1 Interface GUI software.I have connected the EVM with the laptop using the USB cable and able to read/write on I2C. I have connected…
Part Number: TPA2028D1 Other Parts Discussed in Thread: TPA2026D2 Hi,
Could you please tell me the pwm modulation method(AD mode or BD mode or 1SPW mode) for TPA2028D1 ?
Best regards, Kato
Part Number: TPA2028D1 Hi Ti.
My Customer is designing using TPA2028D1.
They are going to use 4Ohm Speaker and 16dB Gain.
Audio source is analog.
Please refer to attached schematic and register setting.
They has two noise issues.
1. When Audio is started…
"I noticed that when I set the fixed gain to max (30dB), over the course of several seconds, the volume increases. It appears that the volume slowly increases up to the value of fixed gain as I repeatedly play a sample sound. Could you explain why this…
Other Parts Discussed in Thread: TPA2028D1 Hi Team, I would like to ask a simple question. Can I limit output power of TPA2028D1 to 0.79Wrms if I only set REG06 register (AGC Control) =1D? I believe it but my customer said he coudn't limit output power to…
Other Parts Discussed in Thread: TPA2028D1 Hi, we are designing the project & need TPA2028D1 reference code fot MTK platform & its porting guide. Thanks!
Other Parts Discussed in Thread: TPA2028D1
Hi Team,
Customer would like evaluate the TPA2028EVM. However, there is unknown issues on customer laptop.
Can you let me know which GUI and driver that customer should use?
e2e.ti.com/.../192135 …
Part Number: TPA2028D1 Hi Team, Is it possible case to damage the device if we apply 0.6V(VIL_max)~1.3V(VIH_min) to EN when VDD=3.6V? Best Regards, Yaita / Japan disty