Part Number: TPA3004D2 Tool/software: HI TI:
The project uses TPA3004D2 and an 8 Ω 2W SPEAKER as the load. 1. When the sound is increased to a certain extent by increasing the gain, the chip enters a protective state with no sound output. 2. No…
Part Number: TPA3004D2 Hi TI,
We have a design to control the 8 ohm speaker using the TPA3004D2. The design schematic is also attached for reference.
When we have a new board, it works fine but when we repeat the tests, after few power cycles, we observe…
Part Number: TPA3004D2 Dear Sir,
We are little bit confused with the datasheet for the TPA3004D2 device . We would like to know whether the 12 Volt Supply or 15 V supply is required to drive the speaker through the IC as mentioned in the datasheet .…
Part Number: TPA3004D2 Dear Team,
For TPA3004D2 can use for higher wattage audio amplifier application like 20,25W and 50W. Below is the image its shows 5-50W.
Other Parts Discussed in Thread: TPA3004D2 , TPA2008D2 Dear Sir
We will use one audio amp solution to design stereo BTL (3W/8ohm) and PBTL (10W/6ohm) ,but PBTL and BTL will not use at the same time
But we need have volume control function just like TPA3004D2…
Hi,
I am planning to use only one input and grounding the other. Grounding one input would result to its associated driver being off. Does that mean that I can leave said associated output pins floating? Specifically, pins 37 to 48? Or are there other…
Other Parts Discussed in Thread: TPA3004D2 Hi,
How works the short-circuit protection on TPA3004D2 ? Datasheet tells that this amplifier is protected against "output-to-output shorts, output-to-GND shorts, and output-to-Vcc short". But we e asily…
Other Parts Discussed in Thread: TPA3004D2 , TPA6110A2 Hi,
I have created a small test PCB to evaluate the TPA3004D2. My application requires a single (mono) speaker with headphone outputs. I used a slightly modified version of the schematic in figure 36…
Other Parts Discussed in Thread: TPA3004D2 HELLO I WILL BE USING THIS DEVICE AS A FRONT END DEVICE FOR A HIGH VOLTAGE FULL BRIDGE LAYOUT I NEED TO SEE IF I CAN GET SOMEONE EMAIL ADDRESS SO I CAN SEND THEM A DRAWING OF HOW I HAVE THE PART LAID OUT TO SEE…
Hi, Ravindra
Analog input, Open loop Class D, you can take TPA3004D2/TPA3002D2 as your reference.
Analog input, Single ended output, you can take TPA3124D2 as your reference.