Part Number: TPA3007D1 We used the Tpa3007d1 component. We set up circuit correctly. Our result voltages are : Vclamp :3.2 v Vref : 4.85 v Vbypass : 2.47 v Vcc : 12 v Shutdown : 12 v Cosc : No Voltage Rosc : No Voltage These are our result. But we didn't see…
Part Number: TPA3007D1 Other Parts Discussed in Thread: TPA3001D1 Hello,
I would like you to confirm about expected observation voltage for following pins when we supply 12V to Pvcc and Vcc.
* Bypass pin (22pin)
* Vclamp pin (7pin)
Best Regards,
Part Number: TPA3007D1
Hi,
I'd like to know the meaning of "21V Compliant" on page3 of TPA3007 D/S.
Does it mean that there is some specific standard and TPA3007 is compliant with it? Or does it simply mean that /SHUTDOWN pin can accept…
Part Number: TPA3007D1 Hi, Is 5pin (Shutdown pin) an internal circuit that increases the current that flows when the voltage is less than 2V? Under the above conditions in the customer's circuit, the current will increase. Best regards, Yuto Sakai
Part Number: TPA3007D1 Other Parts Discussed in Thread: TPA3111D1 , TPA3138D2 Dear sir,
Excuse me.
As title, please help provide TPA3007D1PWG4 θJB( ℃/W) and θJC (℃/W) information for us.
Part Number: TPA3007D1 We have an application with a TPA3007D1 designed in. The application mutes the aforementioned chip until a beep is played. The majority of the chips have worked, but we've had some that take such a long time to come out of mute…
Part Number: TPA3007D1 This is Joong-hyeok Lee, DMSMS researcher of Leoinnovision. Leoinnovision is the official EOL(End Of-Life)/obsolescence part manager of Korean Military (Army, Navy, Air force) and PLM agency of many defense industries (Hanwha, ADD…
Part Number: TPA3007D1 Hi,
I'm using a TPA3007D1 for a mono output audio amplifier. I followed the TPA3007D1EVM schematic to constructed the amplifier circuit. After power up the circuit, I connect the input to an audio source. while plug in the IN+ and…
Other Parts Discussed in Thread: TPA3007D1 Hi~
We will use TPA3007D1 Audio amplifier in BTL mode. As you know, TPA3007 have Gain Control(12dB, 18dB, 23.6dB, 36dB).
We want make 6.5W output power and 1W output power by only gain control at same input level…
Other Parts Discussed in Thread: TLV320AIC3204 , TPA3007D1 Can I connect codec TLV320AIC3204 with TPA3007D1 for transmitting audio signal at a distance of 100 meter.If yes what can be done for conneting mic at the same distance with TLV320AIC3204.
…