Other Parts Discussed in Thread: TPA3106D1 , TPA3100D2 , TPA3101D2 Dear All...,
I really looking a complete circuit diagram for TPA3106D1 IC. Pls forward me if any one is having. It's not that which is in Texas data sheet.
Rohitha
Other Parts Discussed in Thread: TPA3106D1 , TPA3100D2 , TPA3123D2 Dear All...
I'm looking good quality amplifier (FET) which would be stereo input and mono out put. The out put power of 40-50watts RMS. Pls help me
Thanks
Other Parts Discussed in Thread: TAS5186A , TPA2000D1-Q1 , TPA2005D1-Q1 , TPA3100D2-Q1 Hi,
Can the TAS5186A's PVDD supply be anything from 0+ to <40v?
With a higher voltage, the drive capabilities should be higher, but if I limit PVDD to 25v or…
Other Parts Discussed in Thread: TPA3100D2 You may parallel the outputs of Class D amps to achieve 2x the rated output power. We call this configuration PBTL. To do so, you need to half the resistance of the load and maintain the supply voltage. i.e. TPA3100D2…
Thanks Dan!
Correct on the configuration. We have used the TPA3100D2 successfully but now need to up the power. My application has a single 12-24VDC power supply so the TAS56xx series isn't a fit... they are very interesting though!
The gain will…
Andrea, your MODE setting 010 selects BD modulation at the outputs. With BD modulation , when the input signal is zero the outputs switch almost in parallel, with small phase differences that produce narrow alternating differences between the 2 outputs…
Other Parts Discussed in Thread: TAS5613 , TPA3100D2 I have been using the TAS5613PHD2EVM evaluation card and it has been working great in our application. I just noticed that it always operates in BD mode. And it doesn't look like I can test AD mode to…
Matthew, I have attached the presentation that goes with the video. The video itself can be viewed over the video link provided earlier.
The presentation link provided earlier points to a different presentation, a later one on PCB layout for audio quality…
Tomasz, I'm not sure I understand your questions, but I will try to answer. Minimum inductance is indicated on page 4 of data sheet SLES220B, as "Minimum output iInductance at Ioc". It is absolute for the level of Iocp that is programmed…