Part Number: TPA3110D2 Tool/software: I would like to know the dimensions of the TPA3110D2PWP "PWP HTSSOP 28". I had assumed that the size of the rear pad for the "PWP HTSSOP 28" differed depending on the part model, but is this incorrect? Or, if there…
Part Number: TPA3110D2 Tool/software: The datasheet mentions
"peak currents expected for the amplifier"
What is the peak current-draw from the power supply ? I cannot find this info in the datasheet.
I don't mean continuous. I mean brief transients…
Part Number: TPA3110D2
So we have been using this circuit to bias the output signal by using a 12V DC source, however this one is for Single Ended signal while the TPA output is differential.
Reason for asking this is that we want to use a single…
Part Number: TPA3110D2 Hi,
We are developing custom board for one of our client(Audio application).We are using TPA3110D2PWPR Audio amplifier to connect with two 10W speaker.
Below is the issue which we are getting when we powerup the board and send…
Hi Sir,
We found that there is a POP noise when the SD# PIN is enabled.
We attempted to connect an SD# to a button for control. Whenever PVCC and AVCC are active, regardless of when I enable the SD# PIN, it results in a POP noise.
Can you provide…
Part Number: TPA3110D2 Tool/software: Hello, I am Kent. Encountering high temperature issues, please assist. The chip TPA3110D2 is not equipped with a heat sink. When 24V is input, the chip is 65 ℃ under no-load conditions, and the 10uH inductance is…
Part Number: TPA3110D2 Hi,
Could you please review the design of the schematics attached?
I have attached two sheets. The first sheet shows the part being used as a 10W Amplifier for calling purposes. Here, only 1 channel is used. So, is it okay to…
Part Number: TPA3110D2-Q1 Hi,
For TPA3110D2-Q1, doe it can support 8ohm load speaker?
Or TI have other ~10W stereo Class-D AEC-Q100 amp can support 8ohm?
Thanks!
Jeff
Part Number: TPA3110D2 combinepdf.pdf
Hi Team,
I'm using the TPA3110D2 for one of my client projects. We're employing this chip for 2 x 15W audio amplification, with input coming from the Realtek audio codec ALC5616-CGT. However, the TPA3110D2 isn…