Part Number: TPA3110D2 Other Parts Discussed in Thread: TPA3136D2 I use TPA3110D2 in my design, and I do a test --- input sinusoid and measure the output wave of TPA3110D2, the output wave delay 19us than the input wave ,why? and how can I cut down the…
Part Number: TPA3110D2 Dear Sir
We used TPA3110D2 in our new project , in test schedule it had some issue happend.
The sound from the loudspeaker has the noise "pop...pop". The TPA311D2 output connect to the loudspeaker .
We test the wave of TPA311D2…
Hello. 1.The input signal is 100mV in a sine wave. 2.I removed TPA3110D2 which I implemented on a trial manufacture board, and after attaching another TPA3110D2, and examining it, the deficient movement disappeared. 3.This malfunction is thought to have…
Part Number: TPA3110D2-Q1 Hi team,
My customer use TPA3110D2-Q1 in their project. When the DC detect fault is triggered, the fault must be reset by cycling PVCC as shown in the datasheet.
But for the automotive applications, PVCC is always powered…
Part Number: TPA3110D2 Hai ,
We are working on audio Amplifier TPA3110D2 attached is the circuit i am using but I am not able to find any out from speaker,can you please let me know if there should be any change in the circuit I am using
Part Number: TPA3110D2 Other Parts Discussed in Thread: TS5A22364 Hello,
Regarding to speaker input switching on TPA3110D2, my customer is asking a question.
They will switch to speaker input by mechanical relay. (below)
I informed to them the…
Part Number: TPA3110D2 Hello Ti,
This is Sreenath, and I am here to ask about the output power I am trying to generate for my speaker.
Actually I have a Tpa3110 board, and also 4Ohm - 15watt speakers. The main question is that, how can I get 15watt…
Part Number: TPA3110D2 I am using TPA3110D as Class D amplifier to amplify a 90 Hz sine tone. But my output is getting clipped at 2V. I checked PLIMIT pin, the voltage there is at 6.5V, GVDD pin is at 6.9V. First I used power supply of 12V, then 16V but…