Part Number: TPA3111D1 Hello,
I have a design in development with the TPA3111D1 where the output goes through a coupling transformer. With my first prototypes, it worked fine but a newly made prototype produced an asymmetric saturation of the transformer…
Part Number: TPA3111D1-Q1
Dear TI Support Team,
We are facing a recurring IC failure issue in our audio amplifier circuit and would like your support in identifying the root cause and finding a reliable solution.
Initially, we observed audio amplifier…
Part Number: TPA3111D1 Tool/software: I am struggling to understand how to calculate the Plimit voltage based on the datashetet. The values in Table 2 do not make sense to me. I've looked at a few other forum posts, and didn't get any clarity, and the…
Part Number: TPA3111D1 Hi team,
Per datasheet, I see TPA3111D1 has two differential output, can it drive 2 speakers? If can, do we have reference schematic? Thanks!
BR
Jiawei
Part Number: TPA3111D1
Tool/software:
Hello,
My customer is looking for a Speaker Amplifier or solution that supports the following conditions.
- Architecture : Class-D
- Input : Class D PWM
- Speaker channels : Mono
- Output power (W) …
Part Number: TPA3111D1 Tool/software: Hi team,
I have three questions below
[Question 1] If either OUTP or OUTN is shorted to PGND, at which stage does the output become Hi-Z? A. DC Detect (Section 7.3.5) B. Short-Circuit Protection and Automatic…
Part Number: TPA3111D1 Tool/software: Hello,
My customer is asking minimum load resistance in TPA3111D1.
According to Absolute Maximum Ratings(datasheet page 4), minimum load resistance is 3.2ohm.
If it is less than 3.2ohm, what kind of damage…
Part Number: TPA3111D1 Tool/software: Hi team - Based on the related forum post, the discrepancy for the AVCC connections seems to be a known issue. It is still an issue in the datasheet. When will this discrepancy for the AVCC pin functions and recommended…
Part Number: TPA3111D1
Hi, I have one question about TPA3111D1 amplifier.
I have designed PCB according to the datasheet and evaluation board. This is the schematic.
There is one problem with the audio system, which is noise (hum). When there is…