Part Number: TPA3113D2 Hi
Speaker spec 2W/4 Ohm, Expected AMP Gain: set to 20dB Please help tell me how to design AMP? And how to calculate the demand value of Speaker and what should be the input of AMP?
TPA3113.pdf
Part Number: TPA3113D2 Hi Team,
My customer is using TPA3113D2. They get a problem was that sometimes the TPA3113D2 no output after power up , test FALUT pin is low level. Please give me help.
Best regards,
Part Number: TPA3113D2 Other Parts Discussed in Thread: TS12A12511 , TMUX6219 Hi,
I need a audio bridge solution of differential to single_end.See the orange color in below picture.
Could you please help me check if TI has the solution?
Thank you!
Sincerely…
Part Number: TPA3113D2 Hi
2W/4ohm speaker, How to adjust TPA3113D2PWP correctly, Is there a tool to calculate? The attachment is the customer’s current circuit design, in which R416 is currently changed to 1.6K ohm, and the PLIMIT measured is close to…
Part Number: TPA3113D2 Hi TI team,
After reviewing the discussion on the figure shown below, I still got some questions which confused me:
Just a double confirm, if Vin=1Vrms then after a 20dB amp it will turn up to 10Vrms (28.3Vpp)?
As PLIMIT=1.76V…
Part Number: TPA3113D2 Hi,
We need to change the speaker from 4ohm 1.5W to 4ohm 3W. Then what is the plimit value(R459) need to set?
In addition, how to enhance the low bass feeling?
note
the amplifier circuit already reviewed prevent so you don't need…
Part Number: TPA3113D2 Hello,
i'm writing because i have a device developed for us where we use the TPA3113D2 connected to two 1.5W 4ohm speakers. Our problem is that the PVCCR is 5V so the max output power could be (5*5)/4 = 6W and the Vplim is 2.56V…