Part Number: TPA3116D2
Is the output of TPA3116D2 suitable to be boosted to 70v with booster transformer?
I thought of using it for multi room audio where every room has a 70v - 2v step down transformer that feeds a TPA3116D2.
Customized volume…
Hello TI Team,
Thanks for your help. Two questions:
1. Is the TPA3118D2-Q1 available both in the DAD and DAP package?
2. Actually, I would like to ask for thermal models of both the TPA3116D2-Q1 and TPA3118D2-Q1.
Thank you,
Tomasz
Hi Jeff and Ivan,
Thanks very much for your reply. This is a great help in understanding the "clipping" characteristics of this device. "Visually" this looks very similar to the "power limit" capabilities of the TPA3116D2-Q1 device. I purchased the…
Hi,
It seems that TPA3116D2 has two package option, DAD or DAP.
If you look for the CAD file for DAD package, them you can download .bxl file from TPA3116D2-Q1 .
www.ti.com/.../quality
However if you look for the file for DAP, sorry, I cannot…
Hello Yamamoto-san, I think this question directly relates to your last question that I responded to. The TPA3110 has the Speakerguard feature, though it is fairly simple, as an older device, and is likely not the type of protection that you are thinking…
Part Number: TAS6421-Q1 Other Parts Discussed in Thread: TPA3116D2 Tool/software: In one of our projects, we are using the TAS6421-Q1 audio amplifier . With the designed audio file, we were able to achieve the desired power levels (+105 dB(A)). However…
Part Number: TLV320AIC3104-Q1 Other Parts Discussed in Thread: TPA3116D2-Q1
Hi,
We are using TLV320AIC3104-Q1, TPA3118D2QDAPRQ1 and TLV320AIC3100IRHBR in Audio section,
Please find attachment schematic.
Please review all three Pages of schematic…
Other Parts Discussed in Thread: TPA3116D2 [Q1]
Is TPA3116D2 available in the following condition?
<Condition>
・PVcc=15.2V
・RL=4Ω
・Pout=52W
・Output Wave = Square wave
(THD+N = unlimited)
[Q2]
In a condition of Q1,
how much is the…
Other Parts Discussed in Thread: TPA3116D2 Hi,
We have a 5.1 channel application, we use 4 pcs TPA3116D2,
Q1: how to set the master and slave on the 4 parts.
Q2: we now set the bass channel as slave and set other 5 channel as master, the bass channel…
Part Number: LM4752 Other Parts Discussed in Thread: TPA3128D2 , TPA3116D2 Hello guys,
One of my company is considering using LM4752 for their next products.
At this moment,
They have the following questions. Could you please give me your reply…