Part Number: TPA3123D2EVM Hi Audio Team,
The TPA3123D2EVM using shield inductors for L1 and L2 (A7503AY-220M). These have become EOL and my customer is looking into options for replacement.
Do these 22uH inductors need to be shielded? If so, what…
Hi Michael,
I think you could find this info in the TPA3123D2 EVM user's guide:
And the following picture shows the cable which we usually use for the connection between the board and PC.
Best regards,
Shawn Zheng
Part Number: TPA3123D2 Hello,
We are currently evaluating the TPA3123D2EVM to verify the IC’s operation. While checking the gain and frequency response, we observed an unintended gain increase of approximately 50 dB around 250 kHz. We would like to…
Part Number: TPA3123D2 Dears Sirs, I have a problem with TPA3123D2 amplifier. It worked ok, but at this moment when I rise input signal level, the output is cut-off, current consumption latch in 170mA and the chip start hot. I thought the speakers was…
Hi, Ali,
Sorry about that! We have posted the gerbers in the TPA3123D2EVM Product Folder, and the PCB is the same between the two ICs.
You can find the files here: http://www.ti.com/tool/tpa3123d2evm
-d2
I just ordered a TPA3123D2EVM through digikey to test at low frequency, but now I realize that the application diagram in its spwc sheet, and its EVM, have 470 uf DC blocking capacitors on the output, which has a large impact on the low freq response…
Other Parts Discussed in Thread: TAS5613 , TAS5630 , TPA3123D2EVM , TAS5611A , TAS5615 , PCM1808 , TAS5086
The TAS5613 and TAS5630 are capable of delivering considerable power for a distributed 25 VAC audio system. Are these good candidates for achieving…
Hi Yang,
Let me add some comments below:
LC filter can be included, as you mention it would take signal into sine-like wave based on the input signal. No problem with this. Use of filter, either LC or ferrite+capacitor depends on the application…