Part Number: TPA3125D2 Other Parts Discussed in Thread: TPA3122D2 Tool/software: I am considering either TPA3122 or TPA3125 for my hobby project, as I like a DIP (or SO) packages very much, as opposed to thinner pitch ones (I etch my pcbs myself at home…
Part Number: TPA3125D2 I am designing a 5.1 channel audio system using 3 TPA3125D2 amplifiers. The subwoofer has it's own amplifier and will be driven directly from the preamp on my board, meaning that one of the channels will be driven with no load attached…
Part Number: TPA3125D2 Hi
I'm using the TPA3125D2 in Bridge-Tied-Load configuration.
when I configure the Gain resistors, I see that in GAIN (0,0) my signal is very noisy than all the other gains (0,1) (1,0) and (1,1)
the schematics I use are attached…
Part Number: TPA3125D2 Other Parts Discussed in Thread: TPA3136D2 Hi Sirs,
We are survey Audio AMP and Codec.
Our spec inquire as below, could you help to suggest suitable solution for us?
Thanks!!
1. Stereo audio AMP should be capable of driving…
Hi Cameron,
TPA3125D2 supports single-ended input, and there is no minus input. I can't quite understand your question, could you please help to claarify it? Please refer to the datasheet: www.ti.com/.../tpa3125d2.pdf
For 10W output power application…
Other Parts Discussed in Thread: TPA3125D2 Are there design files (Gerbers) for the TPA3125D2 EVM? Could you please point to the correct location?
Thank you in advance
Other Parts Discussed in Thread: TPA3125D2 Hi.
I can't find the max input signal of TPA3125d2. My problem is that with ho input signals the amplifier switch off for a moment and then restart.
Other Parts Discussed in Thread: TPA3125D2 , TPA3123D2 Hi all, Would you mind if we ask AVCC and PVCC of TPA3123D2, TPA3125D2? <Question> The date sheet shows that the value of Min AVCC and the value of Min PVCC are 10V. When the value of AVCC or PVCC…