Part Number: TPA3131D2 Hi,
TPA3131 is filter free class D audio PA, is it ok if I use TPA3131 without LC filter and ferrite bead filter?
And is there any requirement on minimum capacitor need to place on the speaker line?
Best regards,
Zoe
Part Number: TPA3131D2 Hi Team,
We would like to adjust power limit dynamically with the TPA3131D2. Can we do it by changing the voltage on the PLIMIT pin on the fly?
Thanks!
Roy
Part Number: TPA3131D2 What does the absolute maximum slew rate specification for the SDZ, AMx, and MUTE inputs mean?
What happens if this limit is exceeded?
Part Number: TPA3131D2
Hello sir!
I designed used by TPA3131D2 Audio AMP.
My schematic is below that
And FAULTZ pin is direct connected with SDZ pin and connected to VCC_AMP Power with 100kohm resister.
But Audio is not display and FAULTZ…
Part Number: TPA3131D2 Hi Team,
I have one question on the statement below.
"In a single-ended input application, the unused input should be ac grounded at the audio source instead of at the device input for best noise performance"
If ac grounding…
Part Number: TPA3131D2
Can the datasheet conditions of <200uA be drawn externally through the PLIMIT resistor? The datasheet recommends 100k ohm resistors, but can 40k ohm range be used as long as the external current is below 200uA?
Part Number: TPA3131D2 How can I test the 3.4A typical overcurrent trip point on the device for an over current fault? I have tried an OUTNx short to GND and a short across OUTNL/R (load) without being able to create a FAULTZ low. Please advise how to…
Part Number: TPA3131D2 Hi Team,
Customer only need one channel from TPA3131, can we float the output pins?
(BSPL/ BSNL/ OUTPL / OUTNL)
And short INNL and INPL directly to the GND.
Anything else needs to do?
Thanks!
Andrew
Part Number: TPA3131D2 Hi,
We're using TPA3131D2RHBT in our design. "FAULTZ" signal (PIN-30) output is an open drain output ot push-pull output? I'm not able to find relevant details in datasheet.
Part Number: TPA3131D2 Hi team,
Codec output differentially to left channel and Tone voice is output by HPR single terminal in right channel.
When Tone tone works alone, there will be obvious POP tone (Figure 2).
We try to delay PA_Mute for 60 ms…