Part Number: TPA3136D2 Tool/software: Hello,
I am working with TPA3136D2 and would like to clarify a question regarding its duty cycle behavior during output clipping.
According to the datasheet:
9.1 Overview "These capacitors ensure sufficient…
Part Number: TPA3136D2 Hello team,
I received a question from the customer.
The datasheet shows a fixed gain of 26dB, but the customer is considering whether the gain can be changed by adjusting the input resistance value of the differential amplifier…
Part Number: TPA3136D2 Hello team,
I received a question from the customer.
When the LC filter constant is configured with 10uH and 2.2uF, no audio is output. Could you please investigate the cause?
The conditions are as follows.
[1] Based on…
Part Number: TPA3136D2 Other Parts Discussed in Thread: TPA3136AD2 , Hi Team,
May I know the UVLO threshold spec for TPA3136AD2 and TPA3136D2? We can not find it in the datasheet.
Thanks.
Part Number: TPA3136D2 To implement volume control on the TPA3136D2, do i have to place a logarithmic pot on the plimit pin or on the left and right inputs?
Part Number: TPA3136D2 Other Parts Discussed in Thread: OPA2990 Is it possible to close the loop on the TPA3136D2 around an external driver stage?
Can this be done with a PID loop control using an amplifier on each output of the driver stage?
Or could…
I have finally solved my issue. It was a layout issue. The cap connected to pin 11 was not properly grounded.
Adding a wire for this pin to ground solved the issue. Thanks!