Part Number: TPA3156D2 Hi Team,
My customer is using tpa3156. They get a problem on Chip hot in multiple TPA3156 devices work(using the SYNC pin synchronizaing to two amplifiers). When both devices are configured in the master mode, the chip heat will…
Part Number: TPA3156D2 Other Parts Discussed in Thread: TPA3244 Hi,
I want to use the TPA3156D2 audio amplifier in single channel mono mode connected to a transformer from wich the audio goes to multiple speakers.
From reading the post ( https://e2e…
Part Number: TPA3156D2 Hello,
i would like to know, if the gain/master/slave settings are latched after returning from shutdown mode by pulling the SDZ pin high.
The datasheet states at page 14: "The gain setting is selected at the end of the start…
Part Number: TPA3156D2 Hi Sir,
do you share the TPA3156D2 , TPA3116.TPA3118 emission consideration to 30W BTL configuration
especially the ferrite bead to LC redundant solution in EMI .,
is it possible the chamber data sharing(EMI form) for customer…
Part Number: TPA3156D2 I am using the TPA3116 with great success with a 4 ohm load at 24VDC in the mono bridged mode at the lowest gain setting. But when I substitute the TPA3156 it fails catastrophically(thermal runaway) at output levels that that are…
Part Number: TPA3156D2 1. The working voltage of TPA3156D2 is specified under 26V. But we want to use at 28V. Because the charging voltage of 24V battery is 28V.
The charging voltage is designed not to exceed 30V.
Is it OK ?.
2. The attached heatsink…
Part Number: TPA3156D2 Other Parts Discussed in Thread: TPA3116D2EVM Hi Sir,
My customer said they hear inductor noise on their TPA3156's output filter. Would you please helping to check any error or provide suggestion for test/debug? Thanks for your…
Part Number: TPA3156D2 Other Parts Discussed in Thread: TPA3116D2 , TPA3126D2 Customers use TPA3156D2 to do 2*60W. When the sound is maximum, IC enters the state of protection
TI network shows TPA3156D2and TPA3116D2 are pin to pin, it's TPA3116D2's…
Part Number: TPA3156D2 Hello Guys,
Good day!
We have a customer who wants to confirm if they can configure the TPA3156D2 as a single ended output? Also, based on Table 1 in the datasheet, it seems that configuring the device as a unity gain is not…
Hi Adam,
Since we haven't heard from you in a while, we're going to close this post. But if you still need our help as mentioned on prev post, please upload your file so that we can assist you further.
Herman