Part Number: TPA3220 What exactly are the differential and single-ended input impedances for the TPA3220?
The August 2018 data sheet section 9.3.5 quotes impedances of 48k, 24k, 12k, and 7.7k depending on gain selection. It also suggests, but does not…
Part Number: TPA3220 I'm designing a system that will use four TPA3220s in PBTL mode. I'm planning to configure them as slaves and supply an external clock on the OSCx pins, so I can fine tune the PWM frequency and have some insurance against EMI surprises…
Part Number: TPA3220 Other Parts Discussed in Thread: TPA3223 , , TPA3250 It seems that TPA322x and 325x series are quite overlapping in parameters and performance. What is a basic guide to select proper IC for a specific application? Thanks
Part Number: TPA3220 Hi,
in datasheet "AVDD" is connect to +5V and "GVDD" is connect to CRC filter (1uF-3R3-1uF) at +5V, but in EVM "AVDD" is connect to CRC filter (1uF-3R3-1uF) at +5V and "GVDD" is connect to +5V
…
Part Number: TPA3220
Hi team,
My customer found the behavior that TPA3220 output jump up when it is reset.
This is not only 1 product but all product they have, thus it should be product specification.
Please refer to the attached image. Red circle shows…
Part Number: TPA3220 If I want to synchronize the frequency with two TPA3220, GAIN/SLV pin R1 and R2 to set the master and slave, what is effect the FREQ_ADJ pin all connected to 5V direct? I see datasheet slave device FREQ_ADJ connect to 5V, the master device…
Part Number: TPA3220 Hi,
when the AC is off , there is POP sound. We added the mute control circuit, but whenever we put /CMUTE low, the POP sound would come out. There are two problems:
1. Why does /CMUTE turn low to make POP sound?
2. How to solve…
Part Number: TPA3220 Dear Sirs,
I have a project named CEXD-AEIAVB01 and implement the TPA3220 (Output Configuration BTL) for two speakers. Each speaker is 12W, 8ohm.
The PVDD is 12V. The GVDD, AVDD and VDD are 5V. Please see the screenshot below. We want…
Part Number: TPA3220 Good Day,
I have a TI TPA3220 on a custom board along with a TPA3220 Micro Eval kit. The issue that I have been seeing is that in the default pull up state, the value is not the 3.3V as stated but actually 3.9V. It seems as though…