Part Number: TPA3244
Team,
I have two questions about TPA3244:
1. TPA3244 should be able to output 60W on 4ohm load. I am a bit confused why the power power specified in below spec is 25W? What is the difference?
2. What does the peak power in datasheet…
Part Number: TPA3244 Other Parts Discussed in Thread: TPA3221 , TPA3245 Team,
Looks like there is no shut down pin of TPA3244. Could you let me konw how to shut down this device? Thanks.
Regards,
Nic
Part Number: TPA3244 Hi Sir,
There have some question from customer need your support to provide more detail:
1. Did we have the measurement data for PBTL with 8ohm SPK?
2. Could you guide us how to control the volume on TPA3244?
3. Customer would like…
Part Number: TPA3244 Other Parts Discussed in Thread: TPA3220 Dear community members,
There is a problem that initial sound is cut when music is played.
I think that it is occurred due to long precharge time of VIN_X after high /RESET.
So, I want to know…
Part Number: TPA3244 Other Parts Discussed in Thread: DRV135 Amp_TPA3244-B_F_Cu_.pdf
Hello,
i don't get the TPA3244 working. I use 24V and 12V as supply. Inductor: 7447709100 (Würth)
Fault and Clip OTW are both 1. But as soon as i put RESET to…
Part Number: TPA3244 Hi Team,
If I am configuring the TPA3244, what should i do with inputs and output that are not used? If I am driving one speaker or transducer with a single-ended output, should I ground the unused inputs and outputs, or leave them…