Part Number: TPA3245 Hi ti team,
We want to know TI - TPA3245 Inverting voltage gain 's tolerance, please let vendor provide. On the SPEC it is only have Typ value - 18dB.
Part Number: TPA3245 Other Parts Discussed in Thread: PCM1690 ,
Hello all,
im using two of the TPA3245s hooked up to a PCM1690 DAC, all together controlled via DSP/MCU for a well defined startup/shutdown procedure. The last/first thing in this procedure…
Part Number: TPA3245 Other Parts Discussed in Thread: TAS3251 Hi -
I'm working on a design that employs the TPA3245 in pre-filter PBTL mode. In regards to the C_START capacitor, I see this conflicting instruction from the following sources:
Oct 2016…
Part Number: TPA3245 From past work, I'm familiar with the various output filter types that are typically found after the power stages of most class-D amplifiers.
TI's SLAA701A app note, as well as the LC designer tool, reference three filter…
Part Number: TPA3245 Other Parts Discussed in Thread: TPA3255
Hello,
I'm trying to switch between BTL stereo and PBTL mono mode without making any circuit changes other than M1,M2 pins and pulling down INC and IND.
Would it be safe to connect the…
Part Number: TPA3245 Hi TI experts,
My customer asked if it is possible to output 80W on PVDD 24V at load 8ohm. I think it is impossible to calculate.
Using the formula below, it need at least 25.3V for 80W.
P=VI=V*V/R, 80W = V*V*8ohm -> V=25.3V
In…
Part Number: TPA3245 Other Parts Discussed in Thread: OPA1612 , Hello,
I'm planning to connect my DAC through OPA1612 and to TPA3245 like the attached schematic.
And I want to switch between Stereo BTL and PBTL mode without using physical jumpers.…
Part Number: TPA3245 Hello,
While I was designing TPA3245 board, I couldn't find what TVS Diode I needed for ESD protection.
The end of the signal out will be connected to a binding post and probably the speakers will be switched while the device…
Other Parts Discussed in Thread: TPA3245 Hi, we urgently need the user's guide for Amplifier TPA3245 Evaluation Module. Specification AAPO72B SLYFO66A. Thanks a lot for any helping support.
Part Number: TPA3245 Other Parts Discussed in Thread: OPA1622 , TPA3244 , OPA1612 , OPA1632 Hello,
I have one differential Left/RIght audio input and two audio outputs, TPA3245 for a speaker and OPA1622 for a headphone.
I'm trying to keep the cost down…