Part Number: TPA3255-Q1 Other Parts Discussed in Thread: TPA3255 Hello
I woud like to use TPA3255 to drive an ultrasonic transducer up to 60 watt ; the frequency is between 20khz to 32khz .
is this IC suitable for my application ?
I need an impedance…
Part Number: TPA3255-Q1 Other Parts Discussed in Thread: TPA3255 We are testing TPA3255-Q1 and there is a big problem In PBTL Mode I give input signal as 100hz boost from 0 to 1V, load as 4R, when input >=1V Error signal will be triggered low, OTW stay…
Part Number: TPA3255-Q1 Other Parts Discussed in Thread: TPA3255 , TAS5634 Hi,
I am using the tpa3255-Q1 to amplify a 40 kHz signal in BTL mode. I wanted to connect a transducer array to the amplifier and the expected resistance of the array was calculated…
Part Number: TPA3255-Q1 Hi TI customer,
Now we are developing a new D-class audio amplifier box with TPA3255-Q1, but we found the performance are different between different batches. We use professional audio test equipment to test the product, which…
Part Number: TPA3255-Q1 Other Parts Discussed in Thread: TPA3255 1) From my measurements the TPA3255-Q1 itself uses ~6 Watts while running. Are there ways I can decrease the power the chip uses to make it more efficient? It uses 6 Watts whether or not…
Part Number: TPA3255-Q1 Hello Support team,
The specifications do not include the 2Ω output power specification for BTL.
Does that mean you don't guarantee?
Best Regards.
Kaz
Part Number: TPA3255-Q1 Other Parts Discussed in Thread: TPA3255 Hello,
To aim for achieving higher power for one (let's say 4ohm) speaker, can we use multi TPA3255 Amplifiers according to the TI application note for Multi-Device Configuration for TPA3255…
Part Number: TPA3255-Q1 Other Parts Discussed in Thread: TPA3255 Hi, I am using TPA3255 in PBTL Configuration. The output PWM have a big shock in its rising edge, how did it come about and how to deal with it ? Thanks!
The Schematic diagram and OUT_A…
Part Number: TPA3255-Q1 Other Parts Discussed in Thread: TPA3255 , DRV595 Dear:
TPA3255-Q1 , my design is PBTL mode output, input end is INPUT_A,INPUT_B, refer schematic is AC couple, I want to use DC signal input, Could you help give me a suggestion…
Part Number: TPA3255-Q1 Other Parts Discussed in Thread: TPA3255EVM , TPA3255 Hello Support team,
The TPA3255EVM uses the ATS-TI10P-519-C1-R3 heatsink.
The space where the IC is in close contact with the ATS-TI10P-519-C1-R3 is 1.00 mm.
However,…