Part Number: TPA3255EVM Other Parts Discussed in Thread: LM3886 , TAS5630PHD2EVM , TPA3221EVM , TPA3255 , TAS5630 I've designed several Guitar and Bass amplifiers around the LM3886 Cass A/B IC and I check TI website every week hoping for updates for inventory…
Part Number: TPA3255EVM Other Parts Discussed in Thread: TPA3255 Hi,
I' am using TPA3255EVM for testing a piezo actuator driving.
the detailed driving conditions are described as below
- load : piezo actuator, 200nf
- driving frequency 20k ~ 40kh…
Part Number: TPA3255EVM Other Parts Discussed in Thread: TPA3255 , Our customer plans to use TPA3255 to drive DC motor; Motor parameters: power supply voltage is 24V, and the current is about 2A during normal operation. At present, TPA3255EVM is used for…
Part Number: TPA3255EVM Other Parts Discussed in Thread: TPA3255 Dear team,
Our team is implementing a TPA3255 Class D Amplifier for an amplification application involving sinusoids. We plan to use PBTL in order to double power output and reduce temperatures…
Part Number: TPA3255EVM Hi,
We want to boost input gain of TPA3255EVM board after some researchs, i found that if you change R8 and R41 to 20K gain boosts to 2. Is that information correct? If it is not correct please reply with correct solution.
Thanks…
Part Number: TPA3255EVM When I pulled the heatsink off my EVM I found it was not machined correctly and had such a wide space between it and the chip that the heat sink compound did not make contact (thus the chip could overheat).
Part Number: TPA3255EVM Hi, I am using TPA3255EVM in PBTL Configuration(every configuration is set according to the EVM DATASHEET ).
When the input is a fixed value(single-ended input),such as AVDD/2, then I tesed J9 outA ,outB which could see the
…
Part Number: TPA3255EVM Other Parts Discussed in Thread: TPA3255 , TPA3251 , TPA3255-Q1 Does anyone have access to the source files (I think they were done in Altium) for the TPA3255EVM. I would like to use them as a starting point for my application. Thanks…
Part Number: TPA3255EVM Other Parts Discussed in Thread: TPA3255 , , TPA3255-Q1 I have two more questions regarding the TPA3255 and TPA3255EVM.
1. The TPA3255EVM has a 12V regulator for VDD, but the datasheet shows an absolute max rating of 11.4V and typical…
Part Number: TPA3255EVM Hi team,
I got a question from customer about the TPA3255EVM quick start guide.
www.ti.com.cn/.../slou458.pdf
1.running one channel PSTL, how to connect the mono input? do I parallel the mono input to both J3 and J18? can you help…