Part Number: TPA6011A4 Dear TI,
I used TI AMP, the IC is TPA6011A4PWP, please help to review the schematic is there any problem?
Attached file is AMP_TI_TPA6011A4PWP application schematic.
Application: line out to AMP_TI_TPA6011A4PWP through Realtek audio…
Part Number: TPA6011A4 Part number : TI AMP IC-TPA6011A4PWP SMD TSSOP 24P
Issue : The temperature of TPA6011A4PWP-IC rises abnormally when starting up. ask for advice.
Problem Description:
When the MB is turned on with the OS, it will be found that the…
Part Number: TPA6011A4 Other Parts Discussed in Thread: TAS5717 Should it be possible to have a high power (5-10W is enough) similar part with the same interface (headset output, speaker output, output selection based on headset connection, volumen control…
Part Number: TPA6011A4 Dear Sirs,
My customer asked us about function of protection for TPA6011A4.
I found thermal protection in this IC.
So, does this device have protection circuit against load short circuit, ground fault, etc.
Please let me know above…
Part Number: TPA6021A4 Other Parts Discussed in Thread: TPA6011A4 , TPA6030A4 , TPA6047A4 Hi
Because of TPA6021A4N/TI EOL, please recommend if there is a P2P item,
Thank you (
Part Number: TPA6011A4 Hi,
I use the TPA6011A4 to drive dual 4 ohm speaker. I understand the DC bias voltage on amplifier bridge output should be same. (Balance) So no DC current flow through the speaker coil and cause heat. But my issue is: The Amplifier…
Part Number: TPA6011A4 Other Parts Discussed in Thread: TPA2012D2 Hi,
Is it possible to use only one channel of a stereo audio amplifier such as the TPA6011A4, so that is to use it as a mono audio amp.
A follow on question, can such an audio amplifier…
Other Parts Discussed in Thread: TPA6011A4 Dear Sir
We would like to use TPA6011A4 for audio jack application
Could you kindly help to provide the DSN file ??
Thanks
Other Parts Discussed in Thread: TPA6011A4 Hi,
I use the TPA6011A4 to drive dual 4 ohm speaker. I understand the DC bias voltage on amplifier bridge output should be same. (Balance) So no DC current flow through the speaker coil and cause heat. But my issue…