Part Number: TPA6017A2 Hi,
1. Is it possible to drive 8Ω speakers in single end mode?
2. Is it correct to understand that the gain when operating in single end mode is half of the bridged-tied load mode gain?
Best Regards,
Nishie
Part Number: TPA6017A2 Other Parts Discussed in Thread: TPA0212 , TPA6138A2 Hello,
I was using a TPA6017A2 in my design until I realized that the harness where the product will plug in had a single ground and thus expects single ended audio. In my…
Part Number: TPA6017A2 Does this part require termination if an output is unused?
I have a application where we sometimes only use one speaker and one audio channel.
Can i just leave it disconnected?
Thanks
Dave
Other Parts Discussed in Thread: TPA6017A2 when we design TPA6017A2 than it's become over heating and out put become drop, what should I do in this situation?
is TPA6017A2 different with LM4874 ?
pleas advice me
thanks..
Other Parts Discussed in Thread: TPA6017A2 , TPA0152 , TPA0212 , TPA0162 Although it's not listed on the data sheet, the TPA6017A2 does indeed have both these protection circuitries built-in. Both are unlatched faults - which means once the condition…
Hi Michey,
You could have a look at the TPA2012D2 is a Stereo Class-D Audio Amplifier or at the TPA6017A2 is a Stereo Class AB Audio Amplifier. Both devices comply the required conditions.
Best Regards
José Luis Figueroa
Audio Applications En…
Hi, Amy,
We don't have a single-chip solution that supports I2S input and single-ended speaker driver.
So, we have these recommendations:
1. The TPA6017A2 would be a good solution since it supports Class-AB output. This can be used in single…
Hi Weiji Jiang
You could have a look to the following devices: TPA6017a2, LM4838 and LM4836. These devices are designed to work on differential output. Unfortunately, we don't have class AB audio amplifiers to work on single-ended output.
Best Regards…