Part Number: TPA6111A2 Hi,
I'm still working on the mono-to-stereo amplifier application mentioned in an earlier thread ( https://e2e.ti.com/support/audio-group/audio/f/audio-forum/977227/tpa6111a2-non-inverting-configuration?tisearch=e2e-sitesearch&keymatch…
Part Number: TPA6111A2 Hi,
I have a mono-to-stereo amplifier application with a high source impedance. The TPA6111A2 in inverting configuration is loading the source too much, so I was wondering if I could configure it for non-inverting operation by using…
Part Number: TPA6111A2 Other Parts Discussed in Thread: TPA6110A2 , , TPA6110A2-Q1 Hello
Customer wants to evaluate TPA6111A2 and TPA6110A2.
How to get EVM?
Regards
Part Number: TPA6111A2 Hi all,
I have a question about TPA6111A2D.
Is there a specification for the rise time of the High input to the SHUTDOWN pin? Does noise occur when the input signal is steep to the SHUTDOWN pin?
Best Regards, Ishiwata
Part Number: TPA6111A2 Hi,
I'm using TPA6111A2 in the following way, with mono input(Single bulk capacitor) and cascade amplifier configuration. Is this good way to increase the loudness? What is your view point on this?
Regards,
Divya
Part Number: TPA6111A2
Hi,
I am using TPA6111A2 as earphone amplifier. It is working fine. I have mono input and I am using the amplifier in the single ended configuration, which means the power amplification is done by one of the channel. For listening…
Part Number: TPA6111A2 Hi,
I am planning to use TPA6111A2 in audio design, but my audio signal is mono, how can I connect it with TPA6111A2. I have though two way in which I can connect it to IC
1) Giving mono input signal to both audio input
2) Keeping…
Part Number: TPA6111A2 Hi Team,
One of our customer is using TPA6111A and TPA2006 in one of the design and sharing a common input (schematic attached) and both needs to operate in Audio Sectio.pdf parallel can you please help with your comments.
Regards…
Hi Secere,
Thanks for the updates. All TPA611x family are same just different in footprint options. You should just either replace the IC on your current PCB or update the PCB to match TPA6111A2.
Best regards, -Ivan Salazar Applications Engineer