Part Number: TPA6133A2 Other Parts Discussed in Thread: TAD5142 ,
Hi team,
I have two questions.
First, is it okay to connect the TAD5142 and TPA6133A2 as shown below? Additionally, please let me know if there are any precautions I should take when…
Part Number: TPA6133A2 Hi team,
For pins 11 and 14, which are the output lines of the HPAMP IC, would it be acceptable to leave them without any pull-down resistors or other stabilization components for startup?
Based on the EVM schematic, it appears…
Part Number: TPA6133A2 Hi LPA experts,
Do you think it's okay to tie Shutdown pin with DVDD if my customer doesn't need to control shutdown? If you don't recommend, please let me know.
Thanks,
Jay
Part Number: TPA6133A2 Other Parts Discussed in Thread: TPA6130A2 , Hi,
My understanding is that the TPA6130A2 has a similar architecture to the TPA6133A2 but allows the amplifier to work in a BTL configuration via I2C control.
I was wondering…
Part Number: TPA6133A2 Other Parts Discussed in Thread: TPA6130A2 , , TEST2 Hello,
Under long LT situation, we try to develop TPA6130A2 and TPA6133A2 dual support PCB design.
TPA6133A2 Test1 and Test2 pins are assigned SCL and SDA pin in the case…
Part Number: TPA6133A2 Hi,
A customer is considering developing a BT Headset using Qualcom's BLE chipset.
The customer is considering the application of the TPA6133A2 with the Headphone AMP, and has an inquiry.
1. Do you have any history of using…
Hasebe-san,
I apologize for my late response.
The current limiter block is a feature that allows using the TPA6133A2 (and similar devices) without risk to damage the device. Even if the outputs are shorted, the device will be protected.
I have been…
Part Number: TPA6133A2 Other Parts Discussed in Thread: TPA6132A2 , TPA6139A2 , TPA6138A2 , TPA6130A2 hello
how to adjust the output gain of TPA6133A2?
If i just has the single-end input, how to deal with the pin of LEIFINM and RIGHTINM?
Part Number: TPA6133A2 Hi, Support Team
A customer is developing a headset using the TPA6133A2.
During development, the following problems occurred.
1. There is a lot of white noise in the audio output.
2. Amp output is maintained even if…