Part Number: TPA6203A1 Hi Expert,
My customer using TPA6203A in in their project.
Regarding to output voltage noise in specification.
Does hardware portion based on reference circuit ? Especially bypass capacitor.
Also need to know if output noise voltage…
Part Number: TPA6203A1 Other Parts Discussed in Thread: TPA6205A1 Hi team ,
Please provide their ESD information. Thank you.
TI P/N
TPA6201A1DGNR
ESD_HBM
ESD_CDM
Part Number: TPA6203A1 Dear TI Team
I have been asked by our customers for the following information about the TPA6203A1NMBR featured in the TPA6203A1ZQVR EOL Alternatives.
Scheduled product release time
Scheduled update date of data sheet
Could you…
Part Number: TPA6203A1 Hi there,
I am interested to find out if the following components can be used in Class 2 medical devices: TPA6203A1DGNR DRV8837CDSGT INA827AIDGKR LM324DR TPS61099DRVR TPS22910AYZVR TS5A3159DCKR SN74LV1T02DCKR LM321LVIDCKR
Also if it is possible…
Part Number: TPA6203A1
Hi,
It is mentioned in TPA6203A1 data sheet as follows. The input(Ri) and feedback resistors(Rf) set the gain of the amplifier which is recommended to use 1% tolerance resistors or better to keep the performance optimized. So, could…
Part Number: TPA6203A1 Hi,
For TPA6203A1DGNR, TPA6203D1 data sheet mentions the two types of exposed thermal pads dimensions(DGN0008D and DGN0008G) as follows. So, could you please give me your advice about the following questions?
Q1. Which of DGN0008D…
Part Number: TPA6203A1 I am using the Device as per the data sheet. However we are getting the device over heating and failing. I do have a "heatsink via the base of the device soldered onto the pcb tracking, but not to anything else.It looks like thermal…
Hi Sundy,
The biggest difference seems to be that TPA6204A1 has an internal feedback network. You can refer Single-Ended Input Pop Reduction for TPA6203A1 application report to find one way to reduce pop noise. Keep in mind this method is implemented with…
Part Number: TPA6203A1 Other Parts Discussed in Thread: TPA6205A1 Hi,
Could you provide the thermal resistance of junction to package top of DGN?
I would like to know that of TPA6201A1. Datasheet shows only Theta-ja which is converted from derating…