Part Number: TPA6211T-Q1 Other Parts Discussed in Thread: TPA6211A1-Q1 Hello,
I'm checking the details in Section 7.3.2 Fully Differential Amplifier Efficiency and Thermal Information . There's something off with Table 7-1 and Equation 12 . It seems…
Part Number: TPA6211T-Q1 Other Parts Discussed in Thread: TPA6211A1
Hello,
What is the tolerance of the mid-supply (bias) voltage generated by the TPA6211T-Q1 at pin 2 (BYPASS)? (needed for calculating the output bias and peak voltage levels)
Exerpt…
Part Number: TPA6211T-Q1 Hello,
We use a TPA6211T-Q1 to drive a small 8 Ohm speaker, which produces a "beep" sound as an acoustic feedback.
The length of the sound is aprox 56ms. We keep the amplifier enabled only during this time period.
The signal…
Part Number: TPA6211T-Q1 Hi team,
In shutdown mode, is TPA6211T-Q1 Vo biased still active, i.e. biased to VDD/2?
Or bias is also disabled during shutdown? If so, what will be Vo voltage?
Part Number: TPA6211T-Q1 Hi team,
Whether the output pins (Pin5 and Pin8) of TPA6211 support short to ground or short to battery when there is audio signal output or no audio signal output?
BRs,
Haury
Part Number: TPA6211T-Q1 Other Parts Discussed in Thread: TPA6211A1-Q1 , Hi team,
Could you please help confirm if TPA6211A1-Q1 can be used to replace TPA6211T-Q1 on the PCB that with thermal PAD designed for TPA6211T-Q1?
TPA6211A1-Q1 has smaller…
Part Number: TPA6211T-Q1 Other Parts Discussed in Thread: TPA6211A1-Q1 Hi Expert,
Could you pls help comment on the the difference between TPA6211T-Q1 and TPA6211A1-Q1?
BRs,
Wilson
Part Number: TPA6211T-Q1 Hi team,
My customer built prototype for 2022 cluster and having an issue of pop nose when IGN_off (power off the system) .
When turn of IGN, MCU stops audio input to TPA6211 and sets SHUTDONW=Low.
In case SHUTDOWN timing…
Part Number: TPA6211T-Q1 Hello,
we are using the TPA6211 driving a small speaker. In order to get decent sound pressure, we need to lower the input resistor Ri to app. 4 kOhms. We are wondering whether a gain of 10 or even greater is advisable and what…
Part Number: TPA6211A1-Q1 Other Parts Discussed in Thread: TPA6211A1 Hi Expert,
Could you please explain the difference between TPA6211A1 and TPA6211T? Thanks for help!
BR,
Elec Cheng