Part Number: TPA6304-Q1 Tool/software: Hi TI teams,
Above picture is our using block, AMP part name is TPA6304-Q1, there have some power reverse noise go through this red line back to amp when backlight pwm duty is not 100%.
We can hear the tiny…
Part Number: TPA6304-Q1 Tool/software: Hi Team,
We are at present using TPA6304QDDVRQ1 in our design .
Our Question : The Input Signal for the Audio Amplifier has no reduction in clip but the Audio amplifier Output has a clip reduction ( Attached…
Part Number: TPA6304-Q1 Hello:
Please consult, TPA6304-Q1 only uses 2 inputs and outputs. Is it okay to just hang the unused pins? Do you need special treatment?
Part Number: TPA6304-Q1 Tool/software: Hi,
Please kindly approve my Access Permissions for below GUI software, my email is:liang.zhang@arrow.com, thanks.
Part Number: TPA6304-Q1
Tool/software:
Hi Ti,
We are working with Android12 kernel version4.19 integrate Audio amp. we need support from ti Driver part.
Note:
1. Currently we are worked i2cset command based Audio amp validated.
Part Number: TPA6304-Q1 Tool/software: Hello,
We are using TPA6304-Q1 as an audio amplifier.
EVM schematic is attached.
In the EVM board
ASWPA4035S3R3MT Sunlord inductor is used.
The properties of the inductor are attached.
Could we use…
Part Number: TPA6304-Q1 Hello Expert,
One of my customer meets noise issue for TPS6304-Q1 design. Do you mind helping to check their schematic firstly?
The input signal is 70dB while the output signal is 54dB. The SNR can not meet their requirements…
Part Number: TPA6304-Q1 Tool/software: Hi team,
The customer wants to set the address of 6304 to Device0, but the customer also wants the FAULT pin to be connected to the MCU. According to the manual, Fault is an OD gate and a pull-up resistor is required…