Part Number: TPA6404-Q1 We use class D power IC:TPA6404 in my Amplifier product. About the PWM frequency, we set 2.1Mhz. In the 2018 version datasheet, I see that the PWM frequency can only set as 1.8M&2.1M&2.3M.
But in the previous version datasheet…
Part Number: TPA6404-Q1 Hello,
I requested full datasheet from TI request page of TPA6404-Q1 but I could download PurePath software only.
Could you send me complete datasheet ?
And why is complete datasheet not published on web page?
Regards,
Tao_21…
Part Number: TPA6404-Q1 Hello,
My customer is asking about TPA6404-Q1 at PBTL mode
In this mode, can it output 60W power with below conditions?
Conditions:
DC supply(PVDD) : 12V 、
Speaker: load 1 Ω (Mono) ( 0.8 Ω min. )
Output : 60W Max(Mono)
Regards…
Part Number: TPA6404-Q1 Hi Expert,
Our customer want to use TPA6404 to driver Linear amplifier and speaker at the same channel. To sum up, the load is two 4ohm speaker + linear amplifier. The channel works under speaker mode. They don't the detail about…
Part Number: TPA6304-Q1 Other Parts Discussed in Thread: TPA6404-Q1 , Hi ,
Whether there are differences in diagnostics between TPA6304-Q1 and TPA6404-Q1, and whether a comparison list can be provided, thank you
Part Number: TPA6404-Q1 I have followed the TPA6404-Q1 as per the data sheet in PBTL mode:
but can't get any amplification and the red LED is on. Please advise.
Part Number: TPA6404-Q1 Other Parts Discussed in Thread: TPA6404Q1EVM The TPA6404Q1EVM page bears the following link:
CLicking this link earns me an email from customer support, which lets me download and use the PurePath software. This software is…
Part Number: TPA6404-Q1 Hi,
the ch1 of TAP6424 connect the load of 6.8uF&4ohm. customer use AC diagbostic,
set gain =1 I=10mA
read register 0x17 value is 1D, so the Impedance_CH is 29*0.059=1.711ohm.
use Channelx Impedance equlation of 9.3.6.3.3, …
Part Number: TPA6404-Q1 Hi team,
in customer application, the channle 1 and channel 4 of TPA6401 connect tweeter, the channel 2 and channel 3 is connect woofer .
we have below questions:
1. customer use DC load disgnostics, pull down stanby pin and 0x09…
Part Number: TPA6404-Q1 Hi
My customer is asking detail TPA6404-Q1 datasheet but the website version is very limited information.
So could you send complete datasheet then we can forward to customer?