Hello Jeferson:
For a logic signal SE/BTL, I suggest a 0 Ohm Resistor.
The other options, with stuffing options for each case:
TPA701
TPA721
TPA731
TPA741
TPA751 (inverted shutdown so use a stuffing option to Vdd)
There are others…
Other Parts Discussed in Thread: PCM1782 , TPA701 , TPA6205A1 , TAS5342 Hi,
I like to drive a mini speaker (0.3 W nominal, 0.5 W maximal, 8 ohm) after the PCM1782 (mono). It's my first audio application and I am not sure which amplifier I should use…
Did you guys get this resolved? The audio amp schematic looks ok. The 470 pF cap across the inputs will set Fc~13 kHz and will help filtering unwanted high frequency noise. The AIC34 should be able to drive the TPA701 with no problem, considering its…
Part Number: BQ24800 Other Parts Discussed in Thread: TIGER HI
would you help check if our layout has any serious placement or routing problem
below is the schematic (PUA801)
TI-P105_108.pdf
red circle is AGND pin
Regards,
Fred