Part Number: TPD1E01B04-Q1 Other Parts Discussed in Thread: TPD1E01B04
Hello Team,
As E2E post title, does user need to apply serial resistor for POC use case when use protection device TPD1E01B04 ??
I am worry if this affect to channel loss. is this…
Part Number: TPD1E01B04-Q1 Hello,
Could you please provide SPICE Model for TPD1E01B04-Q1 as soon as possible?
Thanks and regards,
Shanjai Kanna S
+91 8072184371
Part Number: TPD1E01B04 Dear support,
Can TPD1E01B04DPYR be used under wave soldering ?
If yes, where can I have the app note for wave soldering spec?
Best regards,Felix
Part Number: TPD1E01B04 I have a question about 8kv-IEC-waveform.
Datasheet waveform and pspice(spice model) waveform are different.
Could you share pspice test sample design?
Test : IEC61000 8KV
pspice result : peak 290V
<Datasheet>
peak 100V
Part Number: TPD1E01B04-Q1 Other Parts Discussed in Thread: TPD1E01B04 Hi Expert,
My customer using TPD1E01B04-Q1 as the ESD protection for FPD-LINK
From customer perspective, on the ESD protection of the high-speed interface, the parasitic capacitance…
Part Number: TPD1E01B04 Dear expert,
I am not able to find the recommended soldering profile and ESD spec (Machine Model) for TPD1E01B04DPYR device.
Can you help to advice?
Best regards,
Felix
Part Number: TPD1E01B04 Other Parts Discussed in Thread: TPD4E05U06 Hi Team,
My customer use our TPD1E01B04 in their high speed signal.
In the datasheet typical application capture, we show that for the USB2 we suggest to use TPD4E05U06.
May we know what…
Part Number: TPD1E01B04 Other Parts Discussed in Thread: SN74LVC1G126 , Hi team,
my customer now have an application scenario. The normal input voltage of the SN74LVC1G126 buffer is 3.3V ( the max voltage on the datasheet is 6.5V ), but the hot-swap device…
Part Number: TPD1E01B04 Other Parts Discussed in Thread: LMH1227 , LMH1228 , Hi support teams,
Our custmer use LMH1227(LMH1228).
If they connect a bad quality SGI cable to connector , LMH1227 was broke down.
Thie reason might be that unexpected voltage biased…
Part Number: TPD1E01B04-Q1 Hi Experts,
My customer is looking for an ESD protection device for PCIE and 10G-Base Ethernet application? Do you have any recommendation? We need automotive part, how about TPD1E01B04-Q1? Thanks.
Arie