Tim-
Your best bet is probably the TPD1E1B04. Since this is on a power rail, the important thing is having a low clamping voltage, and the TPD1E1B04 has one of the lowest clamping with protection up to 30kV which is extremely high. In addition, while…
Hi Yusuke,
Thank you for reaching out to the E2E forum!
For LVDS i can suggest three components that you can take a look into. ESD204 and TPD4E02B04 are both 4 channel bi-directional devices that can handle your data speeds with <-1dB of loss. This…
Hi, JMMN
Customer place TPD1E1B04 on DP and DM pins of all 4 downstream ports of TUSB4041I. They use ESD gun to contact discharge 20kV on the D+ and D- pin (which are connected to pin 33 and pin 34) of the USB socket. The pin 33 and pin 34 of TUSB4041I…
Dustin-
We do not have anything P2P that matches the exact specifications. For a P2P device with lower protection from IEC61000-4-5 surge but still including ESD protection and lower cap, look at TPD1E1B04. For a multichannel solution that meets the…
Hi Kevin,
It would always be ideal if you could clamp the voltage within the abs max listed in the datasheet, but I understand this may not be entirely practical. Some amount of protection like you have mentioned will at least help dissipate the excess…
Hi Takeshi,
Because of the working voltage range being 3.3V and with the given data speeds there are a couple a devices that could be positioned here. The TPD1E0B04 would be one of them as well as the TPD1E01B04, and TPD1E1B04. The biggest difference…
Hi Jay,
Are you connecting the input of the ADC to a 48 V supply directly?
If the line is 3.6 V, than a 5.5 V device works fine. You can use the 3.6 V version TPD1E1B04 .
ESD diodes are most effective close to the ESD source, in most cases the connector…
Hi Sudarshan,
For the 3.3V rails I would recommend the ESD204 which is a 4 channel device like the TPD4E1B06 which you mentioned in your initial question. An advantage of the ESD204 is that it provides EFT protection per the IEC 61000-4-4 standard.…
Hi Alec
Thank you for your reply.
RClamp3391ZC is a single channel device. I tried to compare it with TPD1E1B04 or TPD1E01B04, which are also single channel device but it seems that RClamp3391ZC has better spec than them.
The attached file is the…
Other Parts Discussed in Thread: PSPICE-FOR-TI Back to FAQ Home Page
Interface Protection Guides
Part Recommendation
Packaging & Layout
Models
Transient Standards
System/Device Level Design
Power Dissipation…