Other Parts Discussed in Thread: TPD2E001 Hi! all, Our customer plans to use TPD2E001 and has asked for the S-parameter data for this device. Could you please share the S-Parameter file for this device?
Regards, Toshi
Other Parts Discussed in Thread: TPD2E001 Hi,
I have a question about ESD protection IC TPD2E001.
We will use TPD2E001 and the package is DRS. In TPD2E001 datasheet page.8, there are Layout example for DRL package. But our package is DRS and there are…
Other Parts Discussed in Thread: TPD2E001-Q1 Hi All,
Now our customer has evaluated TPD2E001-Q1 and investigating the failure mode caused by EOS because ESD protection ICs are exposed to outside of system. So that means that there is a possibility of damaging…
HI,
can someone help to answer the question of TPD2E001DZDR ? thanks very much!
1.VRWM (Reverse Stand-off Voltage) 2.VBR(Reversr Breakdown Voltage)@IBR=1mA 3.IR(Reverse Leakage Current)@VRWM=5V
Other Parts Discussed in Thread: TPD2E001 Hello,
The datasheet for TPD2E001 shows that it is acceptable to route an IO trace through an N.C. pin on the 5-pin package. However, for the 6-pin packages, this would connect one IO pin to one N.C. pin, and the…
Part Number: AM3352 Other Parts Discussed in Thread: TPD2E001
Hi Support Team,
We have a defective board that does not recognize USB in a customer's mass-produced product that is a business use printer. The status is as follows.
-A problem occurred…
Other Parts Discussed in Thread: TPD2E001 Hi Our Customer is using the TPD2E001DRLR device in their design.
Some strange thing that they noticed using it:
When there is "high" value on its input lines, the current consumption is around 0.4mA.…
Other Parts Discussed in Thread: TPD2E001 I'm designing a device that has a LiPo battery and a USB connector. USB is used for charging and communication. The on-board microcontroller is powered from either the battery or USB via an integrated 3.3V LDO…
Hello Jimmy,
Unfortunately we do not have the PSPICE model for this part yet. However, if you'd like, you can email me, and we can put this model in our backlog and I can notify you when it's complete.
An existing model you can use for the time…