Other Parts Discussed in Thread: TPD2E001-Q1 Hi All,
Now our customer has evaluated TPD2E001-Q1 and investigating the failure mode caused by EOS because ESD protection ICs are exposed to outside of system. So that means that there is a possibility of damaging…
HI,
can someone help to answer the question of TPD2E001DZDR ? thanks very much!
1.VRWM (Reverse Stand-off Voltage) 2.VBR(Reversr Breakdown Voltage)@IBR=1mA 3.IR(Reverse Leakage Current)@VRWM=5V
Other Parts Discussed in Thread: TPD2E001 Hello,
The datasheet for TPD2E001 shows that it is acceptable to route an IO trace through an N.C. pin on the 5-pin package. However, for the 6-pin packages, this would connect one IO pin to one N.C. pin, and the…
Other Parts Discussed in Thread: TPD2E001 Hi Our Customer is using the TPD2E001DRLR device in their design.
Some strange thing that they noticed using it:
When there is "high" value on its input lines, the current consumption is around 0.4mA.…
Other Parts Discussed in Thread: TPD2E001 I'm designing a device that has a LiPo battery and a USB connector. USB is used for charging and communication. The on-board microcontroller is powered from either the battery or USB via an integrated 3.3V LDO…
Part Number: TMS320F28384S Other Parts Discussed in Thread: TPD4S012 , TPD2E001 Hi champs,
In the F28388D controlCARD, we use TPD4S012 as ESD protection device and the value of serial resistors to USB0DM(R95) and USB0DP(R96) are zero, means we connect…
Below are the latest recommendations of devices for multiple interfaces that provide you IEC protection and paired with low capacitance that minimizes impact to bandwidth in the system. Please also refer to our System-Level ESD Guide for more details…
Other Parts Discussed in Thread: TPD2E001 Hi,
We are considering the TPD2E001 device for a new design, but the package marking is NFGO (it's a marking, so maybe it doesn't really mean anything. However, why doesn't the datasheet list the DZD…
Other Parts Discussed in Thread: PCM2912A , TPD2E001 , TPD2EUSB30A , TPD4S012 , TPD4S014 I am looking at using TPD2E001 for protecting PCM2912A USB interface and VBUS lines. The TPD2E001 datasheet says that its clamping voltage is VCC + 25 and above, which…