Part Number: TPD4E05U06 Other Parts Discussed in Thread: TPD4EUSB30 Hi , Trust you are doing good and safe! Could please suggest the alternate part number for TPD4E05U06DQAR with same footprint (Package) . Thanks , M.Sureshkumar
Part Number: TPD4E05U06-Q1 Hello, my co-workers are trying to understand how the PCB routing is done when using the TPD4E05U06QDQARQ1 in flow-through configuration. We have looked at Figure 13 but have differing opinions. Is it correct in saying that…
Part Number: TPD4E05U06 Hi Sir,
customer used the TPD4EU06DQA on project. found some failure issues of TPD4EU16DQA after the function testing. Please refer to the attachment of the schematics and layout draw. The failure rate is about 20%. Please kindly…
Part Number: TPD4E05U06 Other Parts Discussed in Thread: ESD224 , TPD1E05U06 Hi, I have received the S4P file for the TVS Diode, I connected it to the PCIE +Ve and -Ve lanes. I see that strong connectivity between port 1&3 and 2&4 as shown in fig. I am…
Part Number: TPD4E05U06 Hi Team,
My customer wants to know which process is used in TPD4E05U06, Mesa type or Planar type.
Could you tell me which type is used in TPD4E05U06?
Regards,
Takashi Onawa
Part Number: TPD4E05U06 Hi,
I'm using TPD4E05U06 TVS diode in a project.
D+ / D- pins can be swapped for easy layout routing? Every channel (pin) is individual. Right?
I couldn't see any recommendation about it in datasheet.
Thanks.
Ali
Back to Interface Home Page
DisplayPort Protection
Highlights:
Data speeds up to 20Gbps
8 data lines, 20 total pins
3.3V, 500mA Input
Low capacitance required on data lines
Device
V RWM
Cap
(pF)
ESD(kV)
IEC61000-4-2
Contact
No. of Chan…
Part Number: TPD4E05U06 Other Parts Discussed in Thread: TPD1E05U06 Hi,
Can you confirm the s-parameter port mapping for the TPD4E05U06? The file has two ports - do these correspond to Dx and NC or Dx+ and Dx-. Can you also specify which is the input and…