Part Number: TPD4E001-Q1 Other Parts Discussed in Thread: TPD6E05U06 , TPD6E001 Hello,
I am looking to update our ESD protection solution for one of our EVMs. My application is to protect some ADC pins from ESD, with a stretch goal that it would also help…
Brian,
I apologize for such a long delay.
Using the TPD8E003 would not be be the best idea if there are high speed signals. The IO capacitance of 9pF it pretty high compared to the TPD2E001 and TPD6E001 of 1.5pF.
Regards,
Cameron
Thanks for your swift reply.
22 ohms series resistance is added to MMC0_CLK line
Total Manhattan length of 2279 mils [58 mm] from 22 ohms resistor to SD card connector, Manhattan length from BGA ball to 22ohm resister is 272.29 MIL [7mm]
TPD6E001 ESD…
Part Number: ADS1292R Other Parts Discussed in Thread: ADS1292ECG-FE , , ADS1292 , TPD6E001 , TIDM-BIOSIGNMONITOR Hello I would like to have someone review my schematic for the ADS1292R. I am doing a prototype design for a medical customer. I will readily…
Hi Jonathan,
I'm trying to get these pushed to TI.com but I have attached them here for your use.
Regards, Bill
Daughtercard BOM
am335x_gpevm_gpdboard_3H0001_bom_rev1_2b.xlsx
LCD card BOM
am335x_gpevm_lcdaboard_3H0005_bom_rev1_3a.xlsx
Other Parts Discussed in Thread: TPD6E001 Our company received an AM335x EVM board but it refuses to boot from any SD card.
Obviously, the board should just boot from the supplied SD cards (Linux and Android) and we can clearly see that it does load and…