Part Number: TPD7S019 Hi,
Customer use TPD7S019-15 to replace Onsemi CM2009-02QR, and they test ±3.5KV contact ESD on pin DB15 of VGA.
But they found machines using TPD7S019-15 were black screen or crash. after reset, they work again.
do you have…
Part Number: TPD7S019 Hello Sirs,
May I double check if our CPU Hsync,Vsync,DDC is 3.3V logic or lower .
Can I apply all power supply (Vcc_ddc/Vcc_sync/Vcc_video) to 5V ?
Datasheet application schematic apply 3.3V for Vcc_ddc .
Will sync_in1 & 2 level…
Part Number: TPD7S019 Hi,
Customer raised the question as below.
In the TPD7S019 datasheet, there is a bypass capacitor 0.22uF is showed in function diagram. We do ESD test with 0.1uF bypass capacitor, the test result is pass. Is there any concern for using…
Part Number: TPD7S019 In the datasheet of TPD7S019, I can see a schematic diagram in which TPD7S019 is connected to the output of a VGA controller. Is it possible to connect TPD7S019 to the input of a VGA controller? If yes, how to connect? And is there…
Part Number: TPD7S019 Hi team,
My customer is using the chip as a buffer and cascade 4 chips here. After 4 stages, the influence will be about hundreds mv to make the image has black band. The customer series a 100ohm resistor to the data line to decrease…
Part Number: TPD7S019 Hey Team,
What is the reverse standoff voltage (VRWM) for the TPD7S019? It is mentioned in section 8.2.2 of the datasheet, but I don't see it in the electrical characteristics table.
Best Regards,
Casey
Hi Team,
For the T/TPD7S019-15RSVR, please help to check the capacitor on the application schematic are correct or not.
The capacitor on the application schematic are mF level, However, the description for pin BYP mentioned should use uF level capacitor…
Other Parts Discussed in Thread: TPD7S019 Hi Experts,
May i know what's the maxium DCC signal rate sypported by TPD7S019? I can not find it from datasheet. Thanks!
Best Regards
Fabian