Part Number: TPL0102-100 would you please tell me the failure mode about TPL0102-100? the part in the red circle wil be open or short when a failure happend?
Part Number: TPL0102-100 Hello, My customer would like to use tPL0102-100 at VDD=+3.3V and VSS=-2.5V as following figure. Though the datasheet defines only single supply operation (VDD and VSS=0V) and Dual supply operation (Vss=-VDD) cases, their usage…
Part Number: TPL0102-100 Tool/software: Hi team,
If use dual supply power(VDD=2.75V/ VSS=-2.75V) to power TPL0102 as below, Can I use 3.3V I2C pull up power?
BR
Amber
Part Number: TPL0102-100 Tool/software: Hello,
I am using dual supply operation of TPL0102. Can I use it like this, as given at the below scheme? I need to get -2V to 0V from Wa and Wb.
Regards,
Eren Yildiz
Part Number: TPL0102-100 Tool/software: Is it possible to have both of the channels of the digipot pre-program to a different value other than the default value (127)? If so, what is the process?
Part Number: TPL0102-100 Tool/software: Hi ti team,
When writing I2C data, the pin 6 of TPL0102 experiences a voltage drop, as shown in the figure below. What could be the cause of this issue?
Part Number: TPL0102-100 Hi,
I need help on how to programme the digital potentiometer in Arduino IDE; the libraries and the code. I have connected both channels in series to provide a total resistance of 200k ohms. The code should be able to adjust…
Part Number: TPL0102-100
In our design, it's like the upper circuit. In the application, the VCCD2V0_T of U439 is powered on first, and the LDO is started. The U439 is required to output 1.8V. After 5s, the VDD power of U440 is started (VCCD3V3_DEV…
Part Number: TPL0102-100
In our design, it's like the upper circuit. In the application, the VCCD2V0_T of U439 is powered on first, and the LDO is started. The U439 is required to output 1.8V. After 5s, the VDD power of U440 is started (VCCD3V3_DEV…