Part Number: TPL0102-100 Hi,
I need help on how to programme the digital potentiometer in Arduino IDE; the libraries and the code. I have connected both channels in series to provide a total resistance of 200k ohms. The code should be able to adjust…
Part Number: TPL0102-100
In our design, it's like the upper circuit. In the application, the VCCD2V0_T of U439 is powered on first, and the LDO is started. The U439 is required to output 1.8V. After 5s, the VDD power of U440 is started (VCCD3V3_DEV)…
Part Number: TPL0102-100
In our design, it's like the upper circuit. In the application, the VCCD2V0_T of U439 is powered on first, and the LDO is started. The U439 is required to output 1.8V. After 5s, the VDD power of U440 is started (VCCD3V3_DEV)…
Part Number: TPL0102-100 Tool/software: Hi Team,
My customer is considering the following usage of TLP0102-100.
1. How can the customer estimate the gain tolerance (= ratio of resistance A and B)? Can it be calculated by Rtot.match and MATCHrm? If yes…
Part Number: TPL0102-100 Other Parts Discussed in Thread: TLC555 Dear TI Members,
I'm currently designing a circuit to detect output voltage ripple and need your assistance in selecting the appropriate potentiometer and timer. Here's a brief overview…
Part Number: TPL0102-100 Hi there,
I have recently purchased some of these digital potentiometers.
According to the datasheet, their end-to-end resistance should be 100kΩ ±20%. This means the minimum total resistance should be 80kΩ however multiple of…
Part Number: TPL0102-100 Hi All,
I have a question about TPL0102-100RUC.
Please tell me the changes in Rwl, Rhw, and Rwl over time. Do you have any materials?
Best Regards, Ishiwata
Part Number: TPL0102-100 Other Parts Discussed in Thread: TLV9054 Hi team,
My customer is currently considering using TPL0102-100 pair with TLV9054 in their design with a use case shown as below.
Offset voltage of random level can be observed at the output…
Part Number: TPL0102-100 Other Parts Discussed in Thread: DAC53701 , DAC53204 Hi,
Is it OK for users to connect two digital potentiometers in series? They wants to use two digital potentiometers as 200kohm on TPL0102-100 for LDO output voltage control…
Part Number: TPL0102-100 Hi team
My customer is currently looking for an IC with a similar function: www.analog.com/.../max5417-max5419.pdf
At present, I found that our company's TPL0102-100 has a similar function. I want to confirm with you whether this…