Part Number: TPL0102-100 Hello,
I'd like to first ask if TPL0102-100 can be used for a feedback resistor of a transimpedance amplifier to control its gain. Second, I'd like to know what's the terminal leakage current when both terminals are connected…
Part Number: TPL0102-100 Hi team,
My customer want to use TPL0102-100 in their new project and asked for the bandwidth of this part. The TAM is 100K/Y.
The range of the resistor is 0ohm to 20Kohm, the DS didn't mention the bandwidth calculate method.…
Part Number: TPL0102-100 Hello Team,
Does the TPL0102-100 have a charge pump integrated for EEPROM access? If so is the charge pump only active during read/write of EEPROM or all the time?
Background is a RF design where TPL0102-100 could be used for…
Part Number: TPL0102-100 Hello, Team
according to datasheet page.12
"The TPL0102-100 has an end-to-end resistance of 100 kΩ with a 20% end-to-end resistance tolerance."
it makes TPL0102 20% less accurate, am i understand it right ?
Part Number: TPL0102-EP Other Parts Discussed in Thread: TPL0102-100 , Hi team,
Could you confirm if TPL0102-EP is functionally equivalent to TPL0102-100, except with higher reliability and temp range?
Thanks,
Connie
Part Number: TPL0102-100 Hello Guys,
Good day.
In the datasheet, VIH Maximum Voltage is 5.5V. But at dual supply operation is the maximum value of VIH still 5.5V?
Thanks and regards,
Art
Part Number: TPL0102-100 Dear e2e Support,
My customer uses our DCP in a Safety application.
Could you share what are the different failure modes and related distribution for this TPL0102-100?
Regards,
Part Number: TPL0102-100 Is it OK to configure this device in a "series" configuration by connecting the wiper of the "A" channel with the high side of the "B" channel? Something like this:
I wanted to make it a bit more…