Part Number: TPL0102-100 Other Parts Discussed in Thread: DAC101C081Q Hello, At fast I2C mode, my customer would like to know what could be wrong if tICF (I2C input fall time) is less than the minimum spec, 20+Cb(ns). This spec is originally specified…
Part Number: TPL0102-100 Hello Guys,
Good day.
Our customer wanted to confirm before any programming if the TPL0102 power-up with the wiper settings at mid-point? They would like to verify that it will not start-up in the open resistance state prior to…
Part Number: TPL0102-100 As received, and before any programming, does the TPL0102 power-up with the wiper settings at mid-point? I would like to verify that it will not start-up in the open resistance state prior to programming a value.
Part Number: TPL0102-100 Other Parts Discussed in Thread: TPL1401 hi team,
Customer need Single-channel programmable and burnable digital potentiometer, the interface is preferably I2C. It seems that TPL0102-100 is suitable but it is dual channel. Do you…
Part Number: TPL0102-100 Hello.
1.regarding tolerance of 20% end to end.
does the table list of all the resistance in page 15 are reliable?
2. BIT ASSIGNMENT : BIT 7= VOL, BIT 6=SHDN, BIT 5= WIP .
Does BIT 0,1,2,3,4,5 are register address?
thanks…
Part Number: TPL0102-100 Hi team,
I'd like to know if TPL0102 can keep impedance between H to L, not HI-Z state. As an expectation, remaining 100kohm even in the power down(VDD=0V). From the description below, it can set by SHDN=High. Is it correct…
Part Number: TPL0102-100 We are having multiple failures with this part (TPL0102-100RUCR) on legacy board designs and our technicians cannot find anything wrong with the way it was manufactured. Can TI verify these parts are bad so we can locate where…
Part Number: TPL0102-100 Dear,
we first time use TPL01201-100, could double confirm below schematic.
also we will check resistance will remove R1628
If any suggestion, Please advise me.
Thanks,
Best regards,
Lawrence.
Part Number: TPL1401 Other Parts Discussed in Thread: UCC28086 , , TPL0102-100 Hi,
I want to enquire whether the TPL1401DSGT can be used a a digital potentiometer to adjust the RT pin (frequency) of PWM controller such as UCC28086. If not, do you have any…