Part Number: TPL7407LA-Q1 Other Parts Discussed in Thread: ULN2003A
Hi,
I would like to ensure this is best choice for an application:
For the upcoming design considering using the TPL7407LA-Q1. Is this part a good option for new designs or are there…
Part Number: TPL7407LA-Q1 Hi Team,
There is a good new that we could DIN TI product!
Customer is looking for the replacement of TLE75008-ESD & TLE75602-ESH (P2P would be better )
1. Please help suggest TI solution for the replacement of TLE75008-E…
Part Number: TPL7407LA-Q1 Other Parts Discussed in Thread: TPL7407L , TPL7407LA Dears,
Tpl7407l is used for the seat ventilation heating project . At present, the part damage rate is too high. Customers found the problem is caused by the low level of static…
Part Number: TPL7407LA-Q1 Other Parts Discussed in Thread: TPS1H100-Q1 Hi Team,
There is a good new that Customer is searching TI solution
Do we have a product that can compete with " NCV8452STT1G"?
Part Number: TPL7407LA Hi team,
My customer is considering to use the TPL7407LAD. Could you please support the following questions from the customer?
1. Is there a specification for the power consumption of each CH?
2. Is there a specification for Rds…
Part Number: TPL7407LA Hi team,
My customer is evaluating the TPL7407LAD. Could you please advise to the question below?
During ESD testing, when static electricity is applied to the GND plane, overcurrent or overvoltage may be applied through the GND…
Part Number: TPL7407LA Hello,
I am using the TPL7407LAPWR as digital IO inputs. For UART communication and general inputs. I see in the datasheet that the COM line needs at least 6.3V for optimal MOSFET drive. It does say the following "The COM pin is the…
Part Number: TPL7407LA Other Parts Discussed in Thread: ULN2003A Hi All,
I have a question on TPL7407LA.
What is the MAX value of tPLH below?
What is the maximum frequency that can be input?
Best Regards, Ishiwata
Part Number: TPL7407LATPL7407LA is a driver ic with 7 outputs. The current rating per channel they have mentioned 600 mA per channel but maximum current output mentioned is 500 mA. As it is having 7 outputs if we connect all outputs
in parallel the maximum…
Part Number: TPL7407LA Hello team,
I would like to confirm the pin treatment for this device.
In DS page9, the input could be open if the user will not use the pins because there's an internal pull-down with 1Mohm.
What about output? Can the output…