Part Number: TPS1214-Q1 Hi Team,
I have question on positioning Rsns resistor. As per datasheet the resistor is placed before MOSFET like below.
If we place it after MOSFET as shown in arrow and use only 1 MOSFET Q1, what will happen to output…
Part Number: TPS1214-Q1 Hi Team,
I am using TPS1214, the current sense resistor RSNS is connected between CS1+ and CS1-, this is also shared by other current sensing amplifier will there be any effect of loading or functionality of current sesning.…
Part Number: TPS1214-Q1 Hi Team,
I am using TPS12140QRGERQ1 gate drive and the current monitoring out put we are feeding to ADC of microcontroller.
We would like to know the bandwidth of internal current sensing amplifier and what is the response…
Part Number: TPS1214-Q1 Hi,
I am using TPS12140, while using design calculator I found RSET value to be adjusted for I2T multiplier current. The maximum current mentioned is 100uA. Please refer below snap.
If the IOC=25A, OC_MAX=400A. This 400A…
Part Number: TPS1214-Q1
Tool/software:
Hi Teams,
We are currently testing the OCP function of TPS1214-Q1 and found that after VI2T_OC reaches 2V,
cTMR does not start charging/discharging for 32 cycles. The waveform is as follows. Please help confirm…
Part Number: TPS1214-Q1 Tool/software: Hello,
I am using TPS1214 gate driver. The second gate driver and the bypass path MOSFET I am not planning to use. It will allow load to work in low power mode I guess.
But currently I am using only Main MOSFET…
Part Number: TPS1214-Q1 Tool/software: Hi expert,
If we have device which can support Low Side Current Sense and I2T function? Thanks.
Best Regards,
Ryker
Hi David,
Yes we have many devices that can support current monitoring in addition to current protections.
You can consider TPS4811 or TPS1214 if you need low power mode. Both of these have active current monitoring that can be read by an MCU. TPS1214…
Part Number: TPS1214Q1EVM Other Parts Discussed in Thread: TMS320F28377D , TPS1214-Q1 Hello,
I am using TPS1214Q1EVM for testing purpose. I have few questions.
The SCP_TEST diagnostic feature- Making this signal low to high will perform the internal…