Part Number: TPS1214Q1EVM Tool/software: Dear forum members.
I have a question regarding the TPS1214-Q1EVM evaluation module.
The user guide's "Features" section states "• 3.5V to 40V operating voltage range," while section 1.3 "Specification" indicates…
Part Number: TPS1214Q1EVM Tool/software: Hi Team, We started testing TPS1214Q1EVM. We encountered some problems during testing. We start following the EVM user guide. 1. Short circuit current values not available on the document 2. In Table 2.4, J8 section…
Part Number: TPS1214Q1EVM Hi,
I am using TPS1214EVM board for testing. To do short circuit test I added few external inductors at input side 30uH and at output side 150uH, total 180uH. As the input is 28V di/dt expected is 0.15A/uS.
There are parallel…
Part Number: TPS1214Q1EVM Hi Team,
I am testing TPS1214EVM board. The INP pin is connected through external MOSFET, by default pulled high to VAUX.
In the datasheet it is mentioned that "INP has an internal weak pull down of 100nA to GND to keep…
Part Number: TPS1214Q1EVM Hi Team,
I am performing short circuit test using TPS1214EVM. We have added series inductance to the input line . Below are the test results. The question is we obsered load current going negative after the gate driver has…
Part Number: TPS1214Q1EVM Tool/software:
[Confirmation details]
① I want to know ISC value and variation of immediate shutdown.
② I want to know the variation of IOC
③ Current Consumption of TPS1214Q1
Conditions: at12V, 48…
Part Number: TPS1214Q1EVM Hi,
I the TPS1214-EVM schematic, there are multiple capacitors present like C6, C7, C8, C9, C10.
What is the use of that and is it necessary to have output side capacitor as well like C6 and C7. Currently I am not using output…
Part Number: TPS1214Q1EVM Other Parts Discussed in Thread: TMS320F28377D , TPS1214-Q1 Hello,
I am using TPS1214Q1EVM for testing purpose. I have few questions.
The SCP_TEST diagnostic feature- Making this signal low to high will perform the internal…
Part Number: TPS1214Q1EVM Tool/software: Dear forum members,
I have a question regarding the TPS1214-Q1EVM evaluation module.
I have confirmed that after applying 48V to Vin, it takes approximately 10ms for Vout to appear. Could you please explain…
Part Number: TPS1214Q1EVM Tool/software: Hi,
Is it OK to apply 48V to VIN in TPS1214Q1EVM? As an IC, the operating voltage is 70V, so I think it is okay. I feel that what is written on the first page and the second page of the manual is different. What…